Part Number: LM5141-Q1
I came across this IStep (transient step load current) which is 4A. is IStep assumed value or is there any caluclation involved to get this value as 4Amp.
if any calculations involved please let me know.
Thank you.
Part Number: LM5141-Q1 Other Parts Discussed in Thread: LM5145 , LM61440-Q1 , LM63460-Q1 , 1.Is there any reference circuit with DCR current sensing method-In WEBBENCH tool only current sense method is given
2.How to select HS & LS Mosfet ?-From datasheet…
Part Number: LM5141-Q1 Hi,
can you tell me the difference between Automotive and industrial part for LM1541.We designed for 12V output (Automotive part) output is not coming. output is coming with industrial part.
Part Number: LM5141-Q1 Hi team,
I want to use WeBench to simulate load transient response for LM5141-Q1. But the simulation failed as shown below
How can I fix this?
Regards,
Bengi Long
Part Number: LM5141-Q1 Hello team,
I'd like to use LM5141-Q1 to design a single BUCK with:
Vin: 4V~36V
Vout: 3.3V
Iout: 14A
I understand that t he output current is determined by the power stage componnets (MOSFET and inductor), not the controller…
Part Number: LM5141-Q1 I have a question about inductor selection for LM5141-Q. I checked the required inductor value using two different ways. But I got different results. I am little confused. I would like to know which is correct way to determine the…
Part Number: LM5141-Q1 Other Parts Discussed in Thread: LM5146 , LM5148 Hi Experts,
Good day! We need your assistance regarding the inquiry of our customers below.
In the customer's design, the Vccx-Pin is connected to GND with a 10k resistor. They use…
Part Number: LM5141-Q1 Other Parts Discussed in Thread: LM5141 Hello,
We are using LM5141-Q1 as pre regulator, input is 10V to 32V, output voltage 3.3V
We observed that we have stable output of 3.3V with 4A and we put our ECU to sleep mode where load…
Part Number: LM5141-Q1 Hi Expert:
Because We are testing ISO16750-2 Car battery cold crank test , Vin will drop to 4V with 50mS power supply to LM5141-Q1, LM5141-Q1 Vout is design Vout=3.3V case
but we found Vout will suddenly drop to 1.6V with this…