Part Number: LM5152-Q1 Hi team,
Do "VREF, TRK, RT" pin voltage goes to 0V in shutdown mode? I would like to make sure there is no current comsumption source from these pin.
Regards, Ochi
Part Number: LM5152-Q1 Hi team,
How does boost converter decide its output capacitor? Datasheet says "The recommended VOUT capacitor (CVOUT) is 0.1 μF" but looks too small in general DCDC converter. Should we refer to https://www.ti.com/lit/an/slta055…
Part Number: LM51521-Q1 Other Parts Discussed in Thread: LM5152-Q1 , , LM5125-Q1 , LM5122
Tool/software:
Hi team,
Could we use dual or tripple phase operation by using 2- or 3-pieces of LM51521-Q1? Could you answer the same question for LM5152-Q1…
Part Number: LM51521-Q1 Other Parts Discussed in Thread: LM5152-Q1 , Tool/software: Hello
What are the specifications of the LM5152-Q1?
When the circuit shown in the figure was created with Pspice, the FET operates at 500kHz when voltage V9 is applied…
Part Number: TPS61377 Other Parts Discussed in Thread: LM5152-Q1 Hi support team,
I would like to boost the voltage of a 14.4V lithium-ion iron phosphate battery to 19V. TPS61377 is a candidate, but it would be nice if it also had the Pass-through mode…
Part Number: LM51521-Q1 Other Parts Discussed in Thread: LM5152-Q1 Tool/software: Hello,
I made a design following the "LM5152-Q1_Excel_Quickstart_Calculator_for_Boost_Controller_Design". But my output still has that noise, and I cannot figure out…
Part Number: LM34936-Q1 Other Parts Discussed in Thread: LM5175-Q1 , LM5152-Q1 , LM5176 , LM34936 , LM5175 E2E,
My requirements:
1. AEC-Q100 rated,
2. VIN range: 7.5 to 12.6V
3. VOUT = 12V (fixed)
4. IOUT = 6.27 A max
5. Part must have a…
Part Number: LM5176-Q1 Other Parts Discussed in Thread: LM5152-Q1 , LM5176 , CSD18563Q5A
E2E,
I have a good number of questions though my most pressing question has to due with the compensator components generated by the quickstart calculator and…
Part Number: LM51521-Q1 Other Parts Discussed in Thread: PMP30963 , CSD18536KTT , CSD17318Q2 , LM5152-Q1 , LM5152EVM-BST , CSD17581Q3A , LM5176 Hello Team,
My customer gets the following error (see attached pic) when they try to open the parts reference…
Part Number: LM51231-Q1 Other Parts Discussed in Thread: LM5122 Tool/software: Hello,
I have used the Excel designcalc for the LM5123 but the minimum output capacitance displayed is 3454,50 uF which sounds like a lot. I have done the same calculations…