Part Number: LM5020 Other Parts Discussed in Thread: PMP20777 , LM5185 , , LM5155 , LM5156 , LM51561 , LM51551 Good morning,
I'm looking for find the best Actually TI controller for develop an Isolated Flyback DC/DC controller most powerfull possible…
Part Number: LM51561 Other Parts Discussed in Thread: TL431 , LM5156 Hello, I am prototyping a 50V to 150V DC flyback converter design. First article of the prototype has been assembled but it is not starting up. I believe the converter is encountering…
Part Number: LM5155 Other Parts Discussed in Thread: LM5157 , , LM5156 , LM51561 , LM5158 , LM5156H , LM51561H Hello there:
Since the stock availability is not looking good these days for LM5155, I am wondering if there are some other alternatives…
Hi Koji,
Yes, they can use the LM5156 webench for the basic simulation. But note that they need some additional check.
1. SW and VIN max voltage.
2. Peak current limit
3. Slope compensation
Please let me know if they have any question.
Thanks…
Part Number: LM25184EVM-S12 Other Parts Discussed in Thread: LM5157 , LM25184 , LM5156 Hi Sir,
My customer would like to find an isolated DC/DC converter device for 24V-in to 12V-out / I-out 2A. They also would like to test this EVM to verify the function…
Other Parts Discussed in Thread: LM5156 Hi team,
My customer is designing a 5G outdoor system and they mentioned that the input voltage of system will be -48v.
They need to generate 12 v output and around 5A for system. Do we have suitable reference…
Part Number: LM5158-Q1 Other Parts Discussed in Thread: LM5156 , LM5158 HI,
When I use the WEBENCH Design tool to check LM5158-Q1 with input 6V/ output12V/ 1.2A output current (the same with datashhet reference design).
I find the input and output…
Other Parts Discussed in Thread: LM5158 , TPS61376 , LM5155 , LM5156 Hi, TI support team
The customer wants to design a power supply with the block below.
In order to operate the 7MHz HIFU Transducer using the power of the lithium polymer battery…
Part Number: LM5155 Other Parts Discussed in Thread: LM5156 Is there a way to force the controller LM5155 to work in constant PWM mode and avoid getting to pulse skipping mode operation? On various units having the same design with LM5155 I am noticing…
Part Number: LM34966-Q1 Other Parts Discussed in Thread: LM5156 Hi Team,
Our customer wants to design a power supply using LM34966 with the following specifications.
Minimum input voltage = 8V Maximum input voltage = 24V Output voltage = 150V Power…