Part Number: LM5156EVM-BST The LM5156EVM board is set to work with Vinmax:12V and Vout=12V-3A
However I'd need to change it in order to meet this paramenters:
Vin: 15V Vout: 24V Iout: 1A
What changes do I have to take into account to do this?
Thanks…
Part Number: LM5156EVM-BST Other Parts Discussed in Thread: LM5156 Hi team,
this is UVLO spec in LM5156 EVM
I try to replicate it with calculator but..
but the result show totally different value. (25.886K not 80.6K)
why?
Part Number: LM5156EVM-BST Other Parts Discussed in Thread: LM5156 Hi team,
1.My customer want 65V Vout for monitor application, what should we change aside from the FB resistor on original EVM?
2. would you elaborate any advantage regarding transient…
Part Number: LM5156EVM-BST Other Parts Discussed in Thread: LM5156 I am looking at modifying the EVM to test some design ideas for 200Vdc, with 15Vdc input. I am considering using the output set to 50V, and then using the diode/cap voltage "doubler" to…
Part Number: LM5156EVM-BST Is there a way to allow the EVM to support input voltages greater than 12V? My customer needs to evaluate the part up to 42V. Maybe I'm missing something in the user guide for the EVM. I do see that the IC has a 60V Vin max…
Part Number: LM5156 Other Parts Discussed in Thread: LM5155EVM-BST ,
for EVM: LM5156EVM-BST, or LM5155EVM-BST PCB, :
What is the total thickness ?
What is the thickness for each layer ?
Hello ajayt,
The Altium files for the LM5156EVM-BST have been published at this link under the tab "Design Files" https://www.ti.com/tool/LM5156EVM-BST?keyMatch=LM5156EVM-BST&tisearch=Search-EN-everything&usecase=GPN#design-files
Let…
Hi
This is the right way. This is not a complicated design.
I think you can start with LM5156EVM https://www.ti.com.cn/tool/cn/LM5156EVM-BST . The EVM has similar
And you may also refer to below application note and design calculator.
How to Design a Boost…
Part Number: UCC14240-Q1 Other Parts Discussed in Thread: LM5156 , LM5156EVM-BST Hi Experts,
I am trying to power the UCC14240 from the LM5156.
I am evaluating with the LM5156EVM-BST, but the output ripple voltage is the worst condition of 29.5V( <50ns…