Part Number: TPS55340 Other Parts Discussed in Thread: LM5155 , LM5157 , LM5158 , LM5156 Power product survey
Hello,
The model number is tentatively entered. I am researching power products that meet the specifications below. Could you introduce me…
Part Number: TPS55340 Other Parts Discussed in Thread: LM5157 Hi Team
We are planning to put voltage divider before Enable pin of TPS55340.
We are confused about that 6.5 Electrical characteristics Ven is quite different with the Graph Figure 6-11…
Part Number: LM5157EVM-FLY Other Parts Discussed in Thread: LM5157 Hi Stefan,
The experiments shows that the soft start time of flyback is related with the supply voltage.
In the figure, the blue waveform is the main output voltage. With the supply…
Part Number: LM5158-Q1 Other Parts Discussed in Thread: LM5157 I am trying to use this part in the SEPIC topology. In the data sheet it looks like there are two inductors, but when using the quickstart calculator provided in the data sheet I noticed that…
Part Number: TPS55332-Q1 Other Parts Discussed in Thread: LM5158 , LM5157 Tool/software: Hi,I want to use the TPS55332 in a new design and to do so, I'm trying to understand the example implementation in the section 8.2.1 (datasheet) and I can't understand…
Part Number: LM3481 Other Parts Discussed in Thread: LM5158 , LM5157 Hello, Page 22 of the datasheet, states that the power of the converter can be used in parallel as it will share the current automatically. How can we achieve this performance using…
Part Number: TPS55340-EP Other Parts Discussed in Thread: TPS55340 , LM5157 , LM5155
I used the TPS55340 before, but the internal Fets seem to handle only up to 5A. I need a 8A solution.
Would you have a recommendation for an 8A similar…
Other Parts Discussed in Thread: LM5156 , LM5157 , LM5155 Hi
Please introduce a solution that satisfies the specifications below.
-SPEC-
Input: DC 3.3V~7V ( Battery)
Output: DC 100V 0.001A
Thanks
Part Number: TPS55340 Other Parts Discussed in Thread: LM5157 , LM5158 , , PMP40569
Datasheet says it's isolation-capable.
But I couldn't find option for isolation in webench , or isolated design in the datasheet.
I pasted the webench link here…
Part Number: LM5158 Other Parts Discussed in Thread: , LM5157 , LM5156 , LM51561 Hi,
I'm looking to design a 15V in, 48V out boost circuit.
I've looked at the following parts:
LM5158
LM51581
LM5157LM51571
LM5156
LM51561
I have a few…