Part Number: LM5160 Hey Buck Regulator team,
I have a customer working on a power tree for a new design and we were hoping your team could provide some guidance. Please see a summary of the input/output requirements below in addition to some questions…
Hi Karthik
The voltage drop probably only appears when all of the LDO's start to load the IC. There's 0 current at t=0, so that's why the voltage appears fine at first.
Do you have any flexibility on where the 5V power is located? Is something…
Part Number: LM5160
Hi, (exacte part reference is LM5160DNTJ)
i used Webench design to generate this shematic https://webench.ti.com/appinfo/webench/scripts/SDP.cgi?ID=946C4C28798B699C .
I tried using the same component suggested by Webench and i got noisy…
Part Number: LM5160-Q1 Other Parts Discussed in Thread: LM5160 Hello
i have designed a DC-DC converter and just want to make sure that i have calculated all values right, attached is the schematic for your reference...
input : 19-65V
output: 15V - 2A
…
Part Number: LM5160-Q1 Other Parts Discussed in Thread: LM5180-Q1 , , LM5180 , LM5160 Hello TI expert,
Does LM5160-Q1 / LM5180-Q1's output voltage can directly supply for load ? (because of transformer)
or we need add one additional voltage regulator…
Part Number: LM5160-Q1 Other Parts Discussed in Thread: TIDA-01418 HI,
In reference design of TIDA-01418, about the LM5160QPWPRQ1, I have some question about it:
1. Why it use negative voltage -10.51V to generator 16.8V and 6.27V, but not used positive…
Part Number: LM5160-Q1 Other Parts Discussed in Thread: LM5160 , LMR36520 I want to design flybuck converter with LM5160.
In the application note "Designing an Isolated Buck (Fly-BuckTM) Converter using the LMR36520",there have a suggestion of duty cycle…
Part Number: LM5160-Q1 Other Parts Discussed in Thread: LM5160 , LMR38020 I downloaded a circuit example from the LM5160 product webpage for TINA.
I'd like to ask if on the circuit diagram, "Lmag" refers to the Lpri.
Do I also need to specify…
Part Number: LM5160 Other Parts Discussed in Thread: LM5180 , LM25148 Hi Expert, Is it possible to make LM5160 as ACEQ Complained one? Iam looking for a fly buck controller with integrated switch. could you please suggest the best Controller to convert…