Part Number: PMP10733 Other Parts Discussed in Thread: LM5160 , TPS54560 , PMP22343 Hi team,
I would like to adopt this design; however, some components are seems to be a little old.
Especially, the coupling inductor, TA7848-AE, is very difficult…
Part Number: LM5156-Q1 Other Parts Discussed in Thread: LM5160-Q1 , LM5160 , LM5156 , PMP20904 Hi team,
My customer is looking for a solution:
Input 12V
Output -17V~-24.5V adjustable
Can LM5160-Q1 achieve this?
If not, do you have any other…
Part Number: LM3150 Other Parts Discussed in Thread: LM5160 Hi TI Teams.
①Is it possible to use LM3150 as a Fly-buck?
The primary output is 3.3V/1.5A, second side output is 5V/100mA,±15V/150mA.
②I understand that the requirement for the fly-buck…
Part Number: LM5017 Other Parts Discussed in Thread: LM5160 Hello I'm currently designing a fly-buck based on a LM5017.
My main question is about the low side switch. Do we have to take care of a low side current limit (like in the LM5160) ? Should…
Part Number: LM63625-Q1 Other Parts Discussed in Thread: LM5160 , LM5017 Hi experts,
Is LM63625-Q1 suitable for flybuck design? I checked the datasheet, the negative current limit is -1.8A, which is enough for my application. Is there any limitation…
Part Number: LM5160A Other Parts Discussed in Thread: LM5160 , , TPS54561 Hello,
I want to design 14.8V/ 1.5A power supply by using LM5160A switching regulator IC. My Input voltage will be 28V/4A and my power wattage requirement is 22.2. My only concern…
Part Number: TMS320F280040C-Q1 Other Parts Discussed in Thread: LM5160 Hi,
The customer is using a 35 pin GPIO to control the STB on CAN.
When the MCU STB signal is output to Low, the STB signal remains low and the LM5160 is off.
However, after…
Part Number: LM5160 Hello team
we are using the LM5160 for the Power supply generation of the PWM's Which will drive the IGBT.
But the Problem is that We are getting the all Voltgaes(15V) at the Secondary Side,But when we apply load (10mA) it is dropping…
Part Number: TPS7H4010-SEP Other Parts Discussed in Thread: LM5160 Hi sir,
I have to design a buck converter in IBB configuration in which the input supply is +20V and output is -15V. The load current is approximated to be 0.5A. Which is the best IC…