Part Number: LM5160 Has anyone had any issues with LM5160 evaluation board LM5160DNTFBKEVM?
Using the LM5160 calculator spreadsheet, I modified the following components to model my intended application:
R4 -> 170kΩ (to set ripple voltage feedback).…
Part Number: LM5160DNTFBKEVM Other Parts Discussed in Thread: LM5160 Hi Team,
The customer applying LM5160 in flybuck topology.
They have two problem while testing the EVM:
1. Vout=3V, Vin = 5V,
When VIN = 5V, the output is short-circuited once, the current…
Part Number: LM5160DNTFBKEVM Other Parts Discussed in Thread: LM5160 I trying to design below specification Flybuck DC/DC in the restricted to use LM5160 and 1:1.3 transformer.
⇒Vin: 24V, Vout_iso: 18V / 200mA, Vout_pri: -14V
The reason for Vout_pri…
Part Number: LM5160DNTFBKEVM Other Parts Discussed in Thread: LM5160 Dear TIer,
We are evaluating LM5160 for new projects. However, we find a over current (4.87A) issue at EVM while testing SCP when VIN=5V.
=====
Configuration and Preparation before…
Part Number: LM5160DNTFBKEVM Other Parts Discussed in Thread: LM5160 Hi, I am working on the ISOLATED DC/DC converter using LM 5160 DNT IC.
The design variables are:
Vin= 9 to 36V
Vout = 5 V
Iout = 2A
I got the schematic from the WEBENCH power designer…
Part Number: LM5160DNTFBKEVM Other Parts Discussed in Thread: LM5160 , LM5160DNTBKEVM Hi team,
Regarding LM5160DNTFBKEVM, I am curious to know if this design can withstand a 44V input (rated 32V). I've tested up to 37V without a problem, but before I go…
Hi Tony,
You can probably try to use a flybuck topology, this way you have some isolation between input and output http://www.ti.com/tool/LM5160DNTFBKEVM
The inductor in the buck is replaced with either transformer or coupled inductor. The drawback of…
Part Number: LM5160 hi customer design requirement
3W
1.
Vin=12V~24V(Linear mode)
Vout=5V(isolate)
2.
Vin=12V~24V(Linear mode)
Vout=3.3V(isolate)
3.
Vin=12V~24V(Linear mode)
Vout= ± 15V(isolate)
is LM5160 a suitable solution?
which one of the EVM…
Hello,
When I open the datasheet, I see the output current is rated to 2A.
For example flybuck designs, there are multiple reference designs on the Tools Tab, including: www.ti.com/.../PMP15005. You can also see the EVM with the flybuck configuaration…