Part Number: LMR38010 Other Parts Discussed in Thread: LM5163 Hi team,
Does LM5163 can be directly replaced with LMR38010 without any hardware change? I noticed that the EN &VIN pins are a little different.
Part Number: LM5163 I was able to lay out my schematic but PSpice for TI is throwing a lot of errors when I try to run the simulation.
I have a simulation profile. But curiously, when I edit it, hitting OK doesn't seem to do anything and I have to just…
Part Number: LM5163 Hello, are there any differences between LM5163 and LM5163-Q1? Customer needs to test LM5163 but only LM5163-Q1 are in the sample room. I wonder because there are 2 datasheets.
Regards, Holger
Part Number: LM5163 Other Parts Discussed in Thread: LM5013 , LM5169 , LM5168 , Hi,
My client has buck IC XL7045E1 using XLSEMI, attached is the datasheet.
Pls help to recommend p2p advice. Need DC36V to 5V.
Thanks a lot !
XL7045E1.PDF
Part Number: LM5163 Hello, I have a question concerning the functional block diagram in 7.2.
What is the "bias regulator" in the diagram and what is the function of it ?
Is it designed to convert Vin to 5.5V to power the gate driver of two MOSFET…
Part Number: LM5163 Hi Experts, Good day. Please help confirm what is the actual package drawing dimension of LM5163DDAR. It seems like it is very confusing on the datasheet, especially the thermal pad. Please send the latest drawing. Keep safe. Regards…
Part Number: LM5163 Other Parts Discussed in Thread: BQ76952 , TIDA-010247 Hello everyone! We have developed a BMS with 2 BQ76952 ICs, using the TIDA-010247 reference design. We are using LM5163 IC as a buck converter for the supply. We have observed…
Part Number: LM5163-Q1 Other Parts Discussed in Thread: LM5013-Q1 Hello team,
I received a question from the customer.
If I do not use PGOOD, may I use it as floating? Is it possible to do the same with LM5013-Q1?
Regards,
Masa
Part Number: LM5163-Q1 he below is LM5163QDDARQ1 schematics, please help me to review it, Now the problem is CE( Conduction Emission) issue.
The below figure is the fail .please give the suggestion to reduce the issue.