Part Number: LM5164-Q1 Other Parts Discussed in Thread: LM5164 Hi TI team,
Do we have an example of a good lay-out for the LM5164-Q 1?
Could you please review the lay-out of the figure below?
Thank you.
Kind regards,
Wouter Kragt
Part Number: LM5164-Q1 Other Parts Discussed in Thread: LM5164 , Hi team,
I have designed 48V to 15V converter by using LM5164-Q1 IC, the converter output is 17V instead of 15V, please let me know where is the problem with passive components or LM5164…
Part Number: LM5164-Q1
Hi,
I've downloaded an unscripted Altium library model of the part number LM5164-Q1 and tried transient analysis simulation, but I'm not getting any proper outputs. I've checked all my connections and selection of components more…
Part Number: LM5164-Q1 Other Parts Discussed in Thread: LM5164 Dear Expert
I plan to target this LM5164 by controlling its EN pin to achieve its output and non output, with a control frequency of approximately 20ms of operation and 80ms of rest cycles…
Part Number: LM5164-Q1 Other Parts Discussed in Thread: LM5164 , LM5169 Hello
Im currently using the LM5164 to convert a 48v battery to 13v. While in the normal input voltage range, the input current consumption is around 800uA. However, when the input…
Part Number: LM5164-Q1 I started designing with WeBench a buck converter using the LM5164QDDARQ1. I changed some values to reducde the part diversity in my overall deisgn (See WebenchDesign and Implemented design). With RRON being 47kOhm 1% 100ppm I would…
Part Number: LM5164-Q1 Other Parts Discussed in Thread: LM5164 Dear CC,
In our BMS board we have used LM5164 device. This circuit is design for 12V/1A. But nominal current is only 50mA.
During conducted emission test this is failed even we have removed…
Part Number: LM5164-Q1 Hello, this might be a stupid and embarrassing question but I had to ask because I can't find any info about it.
I was looking at the datasheet and like equation(5) and equation(7), there is (R_FB1 || R_FB2).
What does it mean…
Part Number: LM5164-Q1 Good morning.
We have a design for a +12 SM regulator, (nearly a copy of the reference circuit). This is working well for temperature but the output voltage is affected by the input voltage. The schematic is:
Pos 12V supply.pd…