Part Number: TIDA-00666 Other Parts Discussed in Thread: LM5165 Hi buddy,
In TIDA-00666 designed for BLE transmitter with looped power, could you please help me understand how to provision the power to BLE with less than 3.6mA loop current? in the design…
Part Number: LM5165 Hello, I am planning to use LM5165Y (Fixed 3V3 part) in my design for 0.1A load in COT mode. The input voltage to this part goes as low as 3.4V. Considering Equation 4 of section 7.3.4 of datasheet & considering Inductor's DCR of 0…
Part Number: LM5165 Hello, I am planning to use LM5165Y in COT mode. The load current is 20mA_minimum & 120mA_maximum. Please can you share is there a minimum load current requirement in COT mode for output regulation.
My understanding is that in light…
Part Number: LM5165 Other Parts Discussed in Thread: TPS54040A , Dear TI-Team,
actually we are using the TPS54040A with a Slow Start. The current soft start time is 70ms with a 220nF capacitor. In the datasheet of the TPS54040A it says "The slow start capacitor…
Part Number: LM5165
Hey Expert,
If LM5165 Vout current only have 20mA. Does the output voltage will stable?
We use 12V 15mA power source to be Vin. Vout=5v Thanks for your support.
Jim
Part Number: LM5165 Hi Team,
Due to limited sample, my customer is considering to use LM5165/6X/Y fixed option for 12Vout using Rex like below.
Is it ok to use Rex with LM5165/6XY like below to control output voltage?
Also could you let me know R1/R2…
Part Number: LM5165-Q1 Other Parts Discussed in Thread: LM5165 , LM5156 Hello,
I am willing to design a buck converter based on LM5165 with the next specifications(the calculation file is attached):
Based on LM5156 calculation file and datasheet I made…
Part Number: LM5165 I have questions about the layout for LM5165.
1. Do we need to have the power ground and signal ground?
2. If so, should the power ground connect to GND first or the signal ground should connect to the GND first?
Thanks.
Part Number: LM5165 Hi All
My customer is have trouble sourcing the adjustable version of the LM5165DRC. They would like to add a series resistor into the feedback pin to get a higher voltage output. My questions are , what are the internal values on…