Hello Yuan
Fig 8 and Fig 9 in the Data Sheet for the LM5118 clearly show that Q1 is switching in both the Buck and Buck/Boost modes. This means that its' bootstrap capacitor is recharged at every switching cycle. On the other hand the slyt584 diagram…
Part Number: LM5175
Dears,
our customer reference LM5175 EVM as attached file. 20160614Andy-VehicleBatteryContinuationSystem-M-003_20170808SCH (2).pdf , but our customer find the one question:
system input voltage: 6V~16V , output:12v, CC…
Other Parts Discussed in Thread: TPS55065-Q1 , LM5118 , LM25118 , LM5175 It will be wonderful to have a Texas equivalent for the LT3791-1.
My reason for asking is because I prefer to use a Texas device.
Thank you.
Part Number: LM5176 Other Parts Discussed in Thread: , LM5175 Hi
I have an application for the LM5176.
We are using the controller in a variable output voltage application (achieved by having a DAC add / remove current to / from the VFB pin).…
Part Number: LM5175 Other Parts Discussed in Thread: LM5176 Dear Sir,
could you help review our schematic for attached file.
please let me know that your advisement.
please refer below spec.
Input : DC12V ~ 30Vdc
Output: 14.6Vdc, 20A(max…
LM5175-review-ultraMT-final.pdf
The schematic on p2 is virtually identical to what I laid out.
I made a couple errors in grounding that I can correct with wire, although they won't be grounded as close to the IC as they should.
Vin - vehicle battery…
Part Number: LM5175 hi
in my design i have incorporated the LM5715 as the main power after my battery/charger
the 12v coming out of my LM5715 supplies all the other rails in the board
When i send the CPU to hibernate - most of the board power consumption…
Dear Brigitte,
I replaced my shunt resistors with another model for a test, but always the same behaviour. I shortcircuited the CS and CSG pins bu it do alway the same. I don't understand why!
I used another board with the LM5176, I thought that If…
Part Number: LM5176-Q1 Other Parts Discussed in Thread: LM5176 , LM5175 Dears,
I'd like to request the PCB layout review for two parallel configuration of LM5176-Q1. Please refer to the attached files below.
BMS_PCB Layout.pdf
BMS_LM5176-Q1_Two…
Other Parts Discussed in Thread: LM5175EVM , LM5175 , LM5175RHFEVM-HD Hi All
I have built a power supply using LM5175 using the reference schematic of LM5175EVM.The required output voltage is 12v at 5A. The schematic is attached below. All the components…