Part Number: LM53603-Q1 Other Parts Discussed in Thread: LM61430
Hi Power Management team,
We're looking for a replacement to LM53603-Q1 due to supply constraints. We're using this device as wide input to 3.3V regulator, adding schematic for reference…
Part Number: LM53603-Q1 Other Parts Discussed in Thread: LM53603 Hi Team,
My customer is using LM53603 and asked questions about BIAS pin failure mode.
Q.1) BIAS pin Open
- How LM53603 will behave with this condition?
- Will regulated output be seen on…
Part Number: LM53603-Q1 Hi team,
My customer uses LM53603-Q1 with the configuration similar to Figure 15 of the datasheet with Rbias=4.7 ohm setting.
Q.1) It is required to pass the short-to-GND test for BIAS pin at customer side, the customer would like…
Part Number: LM53603-Q1
Dear all
When I test the load capacity of the device, there is a question about it, as below, my design is according to EVM, Vout set 5V.
1. When my load is 1.4A, then Vin power on, but there is not any output, Why ? the below…
Part Number: LM53603 Tool/software: WEBENCH® Design Tools I want to use LM53603 as a buck converter to step down 5V DC to 3.3V DC. i have noticed in datasheet's application note that everywhere they have mentioned input voltage range as 6V to 36V but…
Part Number: LM53603-Q1 Other Parts Discussed in Thread: LM53603 Hi All,
My customer is using LM53603-Q1 in their T-BOX product and meet EMC issue, so a 10R serial resister was added with Cboot to solve EMC issue. But after adding this resister, we found…
Part Number: LM53603-Q1 I am using the LM53603-Q1 voltage regulator chip with a fixed output voltage of 3.3V and 2.2A max output current. The part works great with an input voltage of 25V but I need it to work down to about 4.5V. The datasheet says it…
Part Number: LM53603-Q1 Hello
We are using LM536035 as a 12V to 5V power supply.When we use the reference design,the DCDC works fine,but the EMC parameters are not good in frequency multiplication.
When we change the value of output inductor,the EMC…
Part Number: LM53603-Q1 Other Parts Discussed in Thread: LM53603 Our customer consider to use LM53603-Q1.
Please advise us following questions.
1. Please send us efficiency data at following conditons if you have.
Ta:-40 degree C,125 degree C
Vin:12…