Part Number: LM5576 Hi team,
[Q1]
Could you tell me the definition of Boost UVLO. Is following correct?
Boost UVLO: UVLO is activated when the BST-SW pin voltage falls below voltage of Boost UVLO.
BOOST UVLO Hysteresis: The hysteresis voltage…
Part Number: LM5576 Tool/software: We have a new board, which is an iteration of a design using the LM5576MHX/NOPB. During testing some of the boards (23/60) have been exhibiting a strange sawtooth wave on the 15V. When the board current draw is measured…
Part Number: LM5576 Tool/software: Hi sir
Design the lm5576 according to the ti tool, measure the IS PIN signal exceeds 2.1 V, and the output current is >7A. The CURRENT LIMIT CYCLE BY CYCLE phenomenon still does not occur. Only the voltage drops from…
Part Number: LM5576 Tool/software: I'm currently in the process of exporting the configuration of an LM5576MHX/NOPB. But the message always appears that the export failed. Is anything known about it?
Part Number: LM5576 Other Parts Discussed in Thread: LM5013-Q1 , LM70840-Q1
Tool/software:
Hello we are looking for a replacement for the LM5576 IC which we have used for a while and seen being used in many UAV power modules to step down till 14S…
Part Number: LM5576 How can the SD pin of the LM5576 in inverting configuration (Vin: 24V, Vout: -18V, Iout: 0.7A) be used? What are the correct connections for AGND, PGND, EPAD?
Best reagrds, Cyrill
Part Number: LM5576 I am doing EMC/EMI for power supplies where LM5576MHX/NOPB is being used for DC-DC step down circuit, where the circuit is not completing its transient analysis , can you help me in resolving this issue.
Regards
Chandana Patil
I am trying to simulate the circuit for 100ms. while doing it TINA TI software is getting hanged. And to reopen the software i will have to close it with the help of task manager.
I have a requirement of running the simulations atleast for 5 minutes…