Hello,
I would still suggest to use the damping capacitor for all EMI scans moving forward since there is a reactive component (LISN).
If you are powering the board up and check DC voltage and regulation, then sure the damping network may not be needed…
Part Number: LM61460EVM Other Parts Discussed in Thread: LM61460 , Hi Team,
What is the difference between LM61460EVM-AS-400K and LM61460EVM-FS-400K ? I guess AS means "adjustable switching" and FS means "forced switching" but LM61460 supports RT(pin 6)…
Part Number: LM61460EVM Hi,
Do you have any transient (0.05A<->6A) test results based on LM61460EVM in PFM mode? i would like to know performance for 3.3V and 5V output.
-A
Part Number: LM61460EVM Other Parts Discussed in Thread: LM61460 Hello,
I'm trying to make a 13.5V with LM61460, but the actual test using the EVM is giving me different results.
I only changed Rt and Rfbb values of the EVM and nothing else.
I started…
Part Number: LM61460EVM Other Parts Discussed in Thread: LMS3655 I'm going to design power board for robotics.
It will be use a battery for VIN, 24~30V, and setted VOUT 24V / 5A.
Could you provide a standard schematic for it?
Thanks.
Part Number: LM61460EVM Other Parts Discussed in Thread: LM61460-Q1 , Hello Team,
I have some questions about LM61460-Q1 EVM.
Q. Regarding with RBOOT resistor, I think adding RBOOT resistor decrease the FET turn on slew rate, then the noise will become…
Part Number: LM61460EVM When powering the evaluation board the supply current is pulling 18mA without any load attached. I have traced the schematic and probed the board, I can not figure out what is causing such a high current draw. Is this expected…
Part Number: LMQ61460 Other Parts Discussed in Thread: LM61460 , , LM61460EVM Hello team,
I have question about input capacitors. In my understanding, LMQ61460 has internal 22nF bypass cap at the each input pin, but LM61460 does not.
I just looked at LM61460EVM…
Part Number: LM61460EVM Hi.
I am using the same schematic as the Evaluation Board with the EMI Filter to output 6V and 6A, I just changed RFBB (R20 on my schematic) to 20K to get to 6V. This schematic with be on a PCB with an MSP432 as well as a GPS receiver…