Part Number: LM6152 Other Parts Discussed in Thread: TINA-TI Hello Team,
With respect to attached differential amplifier circuit
1) what is the minimum differential voltage that can be applied at the input so that the signal gets amplified by the…
Other Parts Discussed in Thread: LM6152 , LM7171 , LM7372 Hi,
I am using lm6152 non inverting, single supply (15v) unity gain design, input 30MHZ 2v pp + changing dc offset.
Outout assumed to be same as input 2v pp +dc offset.
Yet dc Offset ok,…
Part Number: TLE2082 Other Parts Discussed in Thread: LM6152 , LM6172 , TLV9052 , TLV9062 Hello team,
my customer has been using so fa the TLE2082 but is requiring a replacement for it.
Specifically they need:
- package SO8
- Power supply ±12V…
Hi Marceli,
the output current of XTR111 must be limited to less than 50mA or you risk that the XTR111 becomes damaged. The XTR111 is not designed to output a current of 100mA.
I would think about using the improved Howland current pump:
3835.snoa474a…
Part Number: OPA547 Other Parts Discussed in Thread: TINA-TI Team,
We are using the OPA547 for an "improved Howland current pump" to turn voltage to a 0–20 mA output.
It works ok until a given input voltage level. When this input voltage is reached…
Hi Faisal,
A complete discussion of the Improved Howland Current Pump is covered in TI Application Report, SNOA474 (AN-1515), A Comprehensive Study of the Howland Current Pump. That should answer most any question you may have about the fundamentals…
Hey Dan,
LM120K-5.0/883 is indeed obsolete. I've attached the PDN.
We don't have an exact P2P replacement so I'd recommend the UA79 series as the closest alternatives.
~ Aaron
PDN 200824.pdf