Part Number: LM5145 Other Parts Discussed in Thread: TEST2 , LM70860
Tool/software:
Greetings, professionals and forum visitors. I would like to ask your help with LM5145 converter. In my project, converter being powered by 48V Li-Ion battery (input…
Part Number: LM5148 Other Parts Discussed in Thread: LM5145 , LM70860 Tool/software: Hello,
I am going to Design the DCDC power supply and below are the requirements
Input voltage : 48VDC (41 VDC to 57VDC)
Input current : 4.1A
Output Voltage…
Part Number: LM5149 Other Parts Discussed in Thread: LM70860 , LM70660 , LM5148 , CSD19532KTT , CSD19532Q5B Tool/software: I am currently debugging a LM5149 design for a high power industrial application. I am trying to troubleshoot an issue with the…
Part Number: LM5143-Q1 Other Parts Discussed in Thread: LM70860-Q1 , LM5137-Q1 Tool/software: Hello,
My customer is looking for a DC/DC controller solution suitable for developing the following two applications:
They are looking into using the LM5143…
Part Number: LM70880-Q1 Other Parts Discussed in Thread: LM70880 , LM70860 Tool/software: Hello,
My customer requested TI's review of the LM70880-Q1 design.
Please review their design below to see if there are any problems.
LM70880-Q1 REF SCH_20240911…
Hi Daan,
No problem. Yes, the LM70860-Q1 was just released several weeks ago but we should be stocking those devices in the next few weeks.
If there are no further questions, please close the thread by clicking on "resolved". Thanks!
Ben
I was wondering where I can find the quickstart calclulators. Is there one for the LM76003 and LM76002 also? We are also looking at the LM70840, LM70860, LM70880 family of devices. The datasheet does not give the device geometries, and the Webench tool…
Hi Ben,
I got the TI PSpice installed and now when I try to run a testbench example, I get weird errors (see the end of the snippet) and it aborts. Could you guys please help me?
3107.LM70880_V2.0.zip
LM70880_SCH.pdf
** Creating circuit file …