Part Number: LM73 Hello,
I found a tricky description in the 6.1 Absolute Maximum Ratings section of LM73, and I'd like to confirm it.
Voltage at All Other Pins: -0.3 V (Min), (V DD + 0.5 V) (Nom) , 6 V (Max)
I've never seen a nominal value in the…
Part Number: LM73 Hello,
here is my amplifier application. There should be always neagtive voltage on the output, but there isn't...
The problem I have is with negative supply. Ultimately it's supplied with LDO which gives -5V, but until it stabilizes…
Other Parts Discussed in Thread: LM73 I am try to retrieve the Temperature reading through I2c on LM73,,but somehow it give me the invalid value,,,
I am a bit confuse,,,is that register 0x00h is suppose i read out?
Part Number: LM73 Hi Team,
Customer is in urgent to ask for PID (Production ID) /VID (Vendor ID) for Linux Ubuntu Certification, please kindly help, Thanks!
Andrew
Part Number: LM73-Q1 Other Parts Discussed in Thread: TMP100-Q1 , SYSCONFIG , TMP100 I need a reference design to interface LM73C0QDDCRQ1 with microcontroller. Please assist for the same.
Part Number: LM73 Other Parts Discussed in Thread: TMP112 , TMP1075 , TMP102-Q1 , TMP112-Q1 , TMP75-Q1 , TMP175-Q1 Hi sir,
It seemed ok, but I still need your confirm.
What should I take care?
thanks.
Alpha
Hi Jalen,
the customer has reached out with some additional questions:
-------------------------------------------------------------------
we are still struggling with the LM73 improper reset during our system startup. Unfortunately, any HW change is…
Part Number: LM73 Hi,
As the title suggests, I am seeing abnormal temperature readings with the LM73:
- The abnormal readings are not directly after power-on, but after a certain amount of time of valid readings. I have 10 different units and they all…
Part Number: LM73 We have encountered an issue with one of our sensors, where the LM73 (used for PCB temp monitoring) output stuck at nonsense negative value during startup of the system. The analysis identified that proper soft reset was not performed…