Part Number: LM7301 Other Parts Discussed in Thread: OPA197 Hello, I'm trying to add an LM7301 from the default library path ("C:\cds_spb_home\cdssetup\pspTILibDir") to a PSpice for TI schematic page, and though the part is available from the parts placement…
Part Number: LM7301 Please provide the maximum reflow temperature and the time associated with maximum reflow temperature(tp) for SN74LVC1G38DBVR. Please refer to the below image.
Part Number: LM7301 Other Parts Discussed in Thread: TINA-TI Hi Team, Can you help us check the Spice model given for LM7301? We've downloaded the model in its product page but it does not have the proper files, only a MOD file: https://www.ti.com/product…
Part Number: LM7301 Other Parts Discussed in Thread: LM7705 Hi dear expert,
My customer has adopted LM7301 and they have below question: the V+pin will have -0.3V~-0.4V voltage drop for a while before the power is applied. Will this impact LM7301 and…
Part Number: ISO224 Other Parts Discussed in Thread: LM7301 ,
Hello, We have a design using the LM7301 in a follower configuration and a ISO224 to isolate the input from the rest of the circuits. All parts are industrial temperature grade. The primary side…
Hi Robert,
Is there a load on the output of the LM7301? The LM7301 doesn't have much output current drive capability so a heavy load can effect the output voltage. See Figure 13 in the datasheet.
I took a look at the humidity sensor datasheet you…
Other Parts Discussed in Thread: LM7301 Good day,
We have used one TI OPA991IDBVR Operational Amplifier as a unity-gain buffer with the configuration provided below.
We have replaced LM7301 with OPA991IDBVR.
With the current set-up the output of the buffer…
Part Number: LM7301 hi dear supporting team,
how about the max operating Tj of LM7301? from 85degree TA, it seems Tj could not exceed 100 degree. customer is operating at 8V, they normally get 96degree case temp. and the highest case temp could get to 110degree…
Part Number: LM7301 Good afternoon! I am trying to impliment a bandpass filter using the Multiple feedback topology with fo = 19khz, q=20, and Resonant Gain = 40 dB:
Theoretical circuit simulated with a filter design tool, ac magnitude response above…