Part Number: LM7322 Other Parts Discussed in Thread: CSD17308Q3 , OPA2994 , OPA2990 , OPA2991 Sir
I am using LM7322 with dual channels to drive MOSFET
For limiting power dissipation across the MOSFET, we intend to turn off the LM7322 once the allowable…
Part Number: LM7322 Other Parts Discussed in Thread: LM2904B , LMV358A Hi,
We are designing an ac current leakage detection circuit in reference to the below circuit
We found a reference where LM7322 was used for an automotive product.
We are looking…
Part Number: LM7322 Other Parts Discussed in Thread: LM7321 Sir
According to the pin configuration of LM7322 with SOIC package, #1, #5 and #8 defined as N/C
Does the N/C pin have exactly no connection to the internal circuit?
For layout flexibility,…
Part Number: LM7322 Other Parts Discussed in Thread: LM8272 , LM7332 , OPA2992 , OPA2156 , , OPA2994 Hello,
My customer is using the LM7322MM/NOPB. However, there is a problem with delivery.
If there is a newer replacement device that is pin compatible, please…
Part Number: LM7322-Q1 Other Parts Discussed in Thread: LM7322 , TLV9362 Hi,
After applied LM7322 instead of TLV9362, oscillation occurs. We did not observe the symptom with TLV9362.
It's voltage control(inverted voltage) to switch FET gate, and has various…
Part Number: LM7322 Hello,
We are looking atOPA1642AIDGK as a possible drop in replacement for the LM7322MM part, but we do need rail to rail input and output. Do you know if the OPA1642AIDGK would perform well in place of the LM7322MM?
Do you have any…
Part Number: LM7322 Other Parts Discussed in Thread: OPA171 , OPA991 , OPA2994
Hi, Support Team
We will use LM7322 to design AC charging Pile of CFCI function as below chart
have any concern?
if any suggestion, Please advise me.
Thanks,
Best regards,
…
Part Number: LM7322 Hi
I designed a unity inverter with 100K resistors and got conversion factor less than -1 (the actual number was around -0.7)
1. I would like to know what is input resistance of the amplifier between pins 2,3 and 6,5
2. is it Power…
Part Number: LM7322 Hi,
I am evaluating the use of this dual channel Op-Amp in an instrumentation amplifier configuration and wanted to understand the relation of op amp parameters between channels on the same package. Specifically, I wanted to see if…
Part Number: LM7322 Other Parts Discussed in Thread: LM258 , TINA-TI Hi,
I'm using the LM7322 in a non inverting op amp configuration as shown below.
I'm getting output values about 350mV higher than I'm expecting. With a PWM with Von = 5V, Voff=…