Part Number: LM73606 Hi,
We are using LM73606QRNPRQ1 for 24V to 5V conversion. Attached the schematics.
The 24V is given from a custom AC-DC flyback circuit. The 24V ramps up slowly. Hence the 5V is generated before 24V setles down. This intern is powering…
Part Number: LM73606-Q1 Other Parts Discussed in Thread: LM61460-Q1 , , LM73606 , LM61460 Hi Team,
Can you please provide an in-depth (not high level product detail comparison) spec comparison between the LM73606-Q1 and LM61460-Q1?
Thank you in advance!
Hi Thomas,
Thank you for your patience, I've received info that it was tested on a High-K Jedec board which is a 4-layer, so it is probably the 2p2s board.
Regards,
Henry
Part Number: LM61460-Q1 Other Parts Discussed in Thread: LM73606-Q1 Team,
We are trying to promote LM61460-Q1 against our own LM73606-Q1, as LM61460-Q1 is an advanced part. While could you also help to provide a comparison table to show their difference,…
Part Number: LM73606-Q1 In the datasheet for LM73606-Q1 under section 8.3.6 there is an calculation tor P_LOSS_LDO which is the following:
How would I get the I_LDO to calculate this out?
Part Number: LM73606 Hello,
I'm including in my design the LM73606 to generate negative voltage (-4V) rail from positive input (+5V), as related in app note SNVA856B . But i have some open points maybe someone can clarify.
I am not sure how next pins…
Part Number: TPS7H4010-SEP Other Parts Discussed in Thread: LM73606 , Hello,
Is the TPS7H4010-SEP pin-to-pin compatible with the LM73606 automotive/catalog parts? The pinout/package look like a solid match, but the Vin and Vout ratings differ. Do these…
Part Number: LM73606-Q1 I am asking this question on the off chance that there are other satellite designers/users here. My current project is a data processing board for a LEO ESA/UKSA project and I have seen this device being used in a sample PCB picture…
Part Number: LM73606-Q1 Other Parts Discussed in Thread: LM73606 , LM73605 Hello,
The output current for PN: LM73605 5A and for LM73606 is 6A, but they both have the same die, the this die be programmed/modified to adjust the output current?
thank you.
…