Part Number: LM74610-DQEVM Other Parts Discussed in Thread: LM74700-Q1 , LM7480-Q1 Hi Experts,
Seeking your assistance please:
We need OR-ing circuit with Controllers to achieve redundancy with 2 power supply outputs. Attached is the complete power supply…
Part Number: LM74610-DQEVM Other Parts Discussed in Thread: LM74610-Q1 , LM74700-Q1 , , LM74700EVM Hi,
Figure 12 (schematic) on pg. 16 shows using a single FET (SQJ422EP-T1-GE3) per path (FET1_A, FET2_A), which is rated 75A max - If I use 2 x of those FET…
Part Number: LM74610-DQEVM Other Parts Discussed in Thread: LM74610-Q1 Hello,
In LM74610-DQEVM if i gave two different stable solar supply and DC battery 12V 80Ah as an input supply.
what is the output voltage of the evolution board?
means at the out…
Part Number: LM74610-DQEVM LM74610 controller has a FET check function that periodically turn off/on OR'ing FETs for brief moment as indicated in the attached user guide - does it turn off/on both FETs (FET1_A, FET2_A) at the same time or alternating…
Part Number: LM74670-Q1 Other Parts Discussed in Thread: LM74610-DQEVM We are developing a bridge rectifier with ideal diodes. Max current is low (<100mA), AC input voltage 10Vpp.
We were originally going to use the LM74610 device because the datasheet…
Part Number: LM74610-DQEVM HI Sir
We use LM74610 for Oring Diode application
Firstly we turn on 4.3V and than turn on 5V ,but 4.3V power rail will have 5V reverse voltage for a while
Do you have any idea about this issue ?
Part Number: LM74610-Q1 Other Parts Discussed in Thread: LM74610-DQEVM Hi Team,
Our customer will use the LM74610-Q1 in aerospace project. He would like to ask for design review of their schematic diagram which I attached below.
Here are the specifications…
Part Number: LM74610-DQEVM Other Parts Discussed in Thread: TPS24740 , TPS2660 , LM5069 I want to simulate a diode OR configuration combining a main power supply/battery and a small bootstrap battery. The small battery has two diodes in series while the large…