Part Number: LM74610-Q1 Hi,
I'm an EE for General Dynamics and we currently have your Ideal diode (LM74610QDGK) in our designs which works well. We have a new design being implemented that will require we put 750 ohms in series with the input of…
Part Number: LM74610-Q1 Other Parts Discussed in Thread: LM74700-Q1 Hello,
I have come across LM74610-Q1 device for Holdup capacitor circuit application.
We have a diode (for reverse current flow during power down) with Hold up capacitor (3mF) circuit…
Part Number: LM74610-Q1 Hi Experts, Good day. Our customer has the following questions. Please advise.
My case is out of two I am powering only PSU 1 on and Psu 2 is never powered up, well in that case will my overall Oring circuit for PSU1 will work? …
Part Number: LM74610-Q1 Other Parts Discussed in Thread: LM74700-Q1 , LM74700-EP , LM7480-Q1 , LM7481-Q1 We are using LM74610 in a power supply OR-ing application as shown in Figure 21 of the datasheet. However, due to the T0/T1 cycling as shown in Figure…
Part Number: LM74610-Q1 Other Parts Discussed in Thread: TPSM5D1806 Hello
I want to ask you if I use LM74610-Q1 in my application and after that I use switching regulator TPSM5D1806 in my application.
also my input supply is 12v 80Ah tractor battery …
Part Number: LM74610-Q1 Other Parts Discussed in Thread: LM74610-DQEVM Hi Team,
Our customer will use the LM74610-Q1 in aerospace project. He would like to ask for design review of their schematic diagram which I attached below.
Here are the specifications…
Part Number: LM74610-Q1 Other Parts Discussed in Thread: LM74700-Q1 Hi Team,
Could you please confirm that this is the right part number crosses for the following LT device?
LTC4359HMS8#WTRPBF
LM74610QDGKRQ1
Thank you, Delaney
Part Number: LM74610-Q1 I need the LTSPICE model of one component –TI LM74610QDGKRQ1 for simulation.
I download the PSPICE model from TI website but it isn’t work.
I don’t know the reason is TI PSPICE model doesn’t adapt LTSPICE or the…
Part Number: LM74610-Q1 Other Parts Discussed in Thread: LM74700-Q1 I am going to use this part to protect against reverse polarity scenarios, etc.
The power input is 24V and maximum 3 amp load.
How to choose the correct Mosfet for this scenario?