Part Number: LM74700-Q1 Good morning, I'm considering to use the IC LM74700-Q1 in order to protect our battery-operated devices against accidental polarity reversal. Our device use 12Vdc battery, voltage can vary from 14 to 10 Vdc. The nominal current…
Part Number: LM74700D-Q1 Good day. I trust you are doing well? We are busy with a design where we wish to use the LM74700 for reverse current protection on the input. Where I am a bit concerned is that TI suggests to choose (20 mV / ILoad(Nominal)) ≤ RDS…
Part Number: LM74700-Q1 Other Parts Discussed in Thread: LM5050-1 Hi there
we are going to design E - FUSE board (based on the TPS48110-Q1) for protecting on 48V DC motors
one of the problem we faced is that the regenerated voltage comes from those motors…
Part Number: LM74700-Q1 I want to add reverse polarity protection on a 48V line with 200A . In order to keep the losses at a minimum for thermal management, the MOS requirements are proving to be a hiccup . Is there any alternative design mechanism which…
Part Number: LM74700-Q1 Hello, I am working in Robert Bosch Germany for Automotive Electronics Hardware development with Functional Safety.
For one of our new design we need Un-Encrypted PSpice model of LM74700QDBVRQ1. We will use it inside Saber.
I hope…
Part Number: LM74700-Q1 Would like to use this on a power supply for reverse polarity protection, would TI please provide me an unencrypted model?
Thanks
Part Number: LM74700-Q1 Other Parts Discussed in Thread: LM74502-Q1 , , TPS25961 , TPS2521 , TPS25947 , LM74800-Q1 , TPS2663 , LM76202-Q1 Simple question - I'm considering using the LM74700QDBVRQ1 as a NMOS power (DC) switch controller. Can I connect the…
Part Number: LM74700-Q1 Hi Team,
May I know whether we have PSpice model based on LM74700-Q1 which combine the ISO7637-2 pulse 1 and 3a testing?
I mean the simulation file already have the power source which can simulate the behavior of ISO7637-2 pulse…