Part Number: LM75A Customers have asked the following questions to register their products. Can you give me more details?
Material:LM75AIMME/NOPB
1. Use Ni for grounding or not. : Yes / No
2. Thickness of outermost layer plating : 10 μm or more / Less…
Part Number: LM75A Hi expert,
LM75A DS shows that the temperature accuracy but do we have accuracy over time data e.g. 5-10yr can share as well?
Regards,
Allan
Part Number: LM75A Hi Team,
My customer has a question.
The other devices that uses same I2C bus as LM75A is required for I2C clock stretching .
Clock stretching doesn't affect the operation of LM75?. LM75 work properly? Thanks,
Shoo
Part Number: LM75A Hello E2E,
Our customer is trying the LM75 with there test board. When they written 0x3C00 to Thyst register, the device output 0x3CFF when read. Is it malfunction? Or is there a problem with how to use it?
Best regards, ACGUY
Part Number: LM75A Hello.
We consider to use this PN for space low orbit application. Please let me know if you have performed any radiation screening on these parts.
Thank you in advance, Michael
Hi Sunney,
The LM75A datasheet specifies I2C operation up to 400kHz. Although the design may be working fine, we cannot guarantee operation outside of what is shown in the datasheet.
Best regards,
Jesse
Part Number: LM75A Other Parts Discussed in Thread: LM70 , LM75B , LM73 Hi Sir,
May I know the heat flow used on LM75A which pin-out?
Temperature sensors: PCB guide lines for surface mount devices: https://www.ti.com/lit/an/snoa967a/snoa967a.pdf
Part Number: PROCESSOR-SDK-AM335X Other Parts Discussed in Thread: LM75A , AM3352 , SYSCONFIG
Hi,
We are using LM75A temperature sensor to measure the temperature value of our custom board.
LM75A Temperature is directly connected to am3352 I2C0 bus using…
Part Number: LM75A Other Parts Discussed in Thread: TMP1075 Hi Team,
The datasheet of LM75A mentioned the Configuration Register of D5~D7 as below:
D5–D7: These bits are used for production testing and must be kept zero for normal operation.
My…