Part Number: LM79 Hi, Good day. Our customer would like to clarify about the output current of LM7912. I am looking at a 7912CT/NOPB data sheet. On the first page in the features and description is notes a 1.5A output current,
in the electrical specifications…
Part Number: UA78 Other Parts Discussed in Thread: LM79 , UA79 ,
Hi all,
I would like to know the difference between UA family and LM family.
UA78 and UA79 family become EOL, So my cutomer will replace UA family to LM78, LM79 family.
Are there any distinctive…
Part Number: LM79 Hi team,
My customer provided a question in terms of thermal resistance of LM7915CT/NOPB.
LM79xx specifies typ and max θjc on page 4.
Does the θjc mean junction-to-case (bottom) thermal resistance?
Best regards,
Shota …
Part Number: LM79 Recently i got some issues with a competitor LM7915 part. It stays at 0V output voltage, if input voltage is higher then 27V and turned on rapidly. Rapidly means input voltage rises faster then the output voltage, creating a short period…
Part Number: LM79 Hello support team,
I have a question about the LM79xx series.
According to the datasheet of LM79xx, the output noise voltage is typically 300 μV. And its frequency condition is 10 Hz ≤ f ≤ 100 Hz. Isn't it a mistake of 10 Hz…
Part Number: LM79 Other Parts Discussed in Thread: LM2990 Hello experts,
I'm looking for 3-terminal regulator (TO-220) with fixed -15V output.
LM7915 looks good, but operating temperature range is little bit narrow. I need the device which can support…
Part Number: LM79 Other Parts Discussed in Thread: UCC284 Hi, I've checked both LM and UA series LDO but can't find an industrial grade one.
Do we have such device, do we have plan to release such device?