Part Number: LM9061 Dear TI team
Is the following understanding correct when using "LM9061"?
Please advise if there are any other points to consider.
① The "ON/OFF" pin of "LM9061" can be asserted at a voltage -0.3V lower than the "Supply…
Part Number: LM9061 Other Parts Discussed in Thread: LM5060EVAL , LM5060 Hi Experts,
I wanted to try LM9061 as a b idirectional switch with reverse overcurrent protection from the datasheet page 24 and the picture below:
I noticed undesirable behavior…
Part Number: LM9061 Other Parts Discussed in Thread: TPS4811-Q1 Hi experts,
Is the time for LM9061 input rising edge to switch conduction this Ton 1.5 ms? (Delay = 1.5ms?)
Why delay is so high? (ADI's high side driver LTC4440 takes about 50ns, customers…
Part Number: LM9061-Q1 Dear sir,
I am planing to using the LM9061-Q1 ic for reverse polarity protection. This ic suitable for the reverse polarity protection or any other ic are there?
Our requirements:
Voltage: 400V DC
Current:7.5A
Power: 3KW
Part Number: LM9061 Other Parts Discussed in Thread: TPS4811-Q1 Hi,
I'm using LM9061 as a load switch driver to control an external MOSFET. I have few questions:
Can I use LM9061 to control two parallel MOSFETs?
My supply voltage (at pin 2 of LM…
Part Number: LM9061 Other Parts Discussed in Thread: LM5060-Q1 , LM74800-Q1 , LM7480-Q1 , Hi Team,
Good day! I am posting this in behalf of the customer.
I have shared the full details of inquiry below:
My new project is to design an electronic master switch…
Part Number: LM9061-Q1 Other Parts Discussed in Thread: LM5067 Hi, support team
My customer has the questions as follow:
I am looking at your LM9061-Q1 product and I want to use to for its features. However, the datasheet of this product showcases an…
Part Number: LM9061 Other Parts Discussed in Thread: LM5060-Q1 , LM5060 Hi,
I have a couple of questions regarding the LM9061:
1. The quiescent current is too high for my application (5 mA when OFF). Can I disconnect the power to the device after issuing…
Part Number: LM9061-Q1 Other Parts Discussed in Thread: TPS25982 Dear Sir,
Currently, I am using LM9061M_NOPB
Do you have a similar IC which works for Supply voltage: 6V to 9V DC.
Regards Murthy
Part Number: LM9061-Q1 Other Parts Discussed in Thread: LM9061 , LM5069 , LM5066 , LM5050-1-Q1 , LM5060-Q1
Dear Sir,
I am using LM9061 for hotswap of two supplies from mains and Battery,to swap the Voltage of 24 Volt. I am using two LM9061 to drive two mosfets…