Part Number: LM95172-Q1 Please tell me about a Reflow profile of lm95172-Q1.
Data sheet page3 aboslutte maximum ratings spec Soldering Information Infrared or Convection (20 sec.) 235℃
It is written in this way
Reflow peak 235℃ 20sec??
Dear Gnana -
We have plenty of parts which meet your speed, accuracy and package requirements, but the max temperature you specify is problematic for most semiconductor packages and most are soldered down using 260C peak. We do have one part rated to…
Part Number: TMP468 Other Parts Discussed in Thread: LM95172-Q1 Hi TI Team, We have a requirement of I2C based Temperature Sensor that can measure ~180-190 deg. C. We can have a BJT-based remote sensing approach. We have selected TMP468 for our application…
Other Parts Discussed in Thread: LM95172-Q1 Hi Kunal,
Hope you are doing well.
I want to test the temperature in-between the Tyre threads. Can you please let me know which sensor should I choose.
Thank you,
Kyza.
Hi Aaron, Thanks for your support. But the customer needs the sensor that can measure 0~200 °C. TMP107 can only measure -55°C to 125°C. It cannot meet the customer's requirement. Do we have any other temperature sensor?
I found there…
Hi Abhishek,
With the HDC1080, the temperature range that can be measure is from -40 to 125°C.
For temperaure sensor that works at higher temperature you can take a look to the LM95172-Q1 , that works until 200°C, but if you need more information about…
Hi Michel,
Thank you for your inquiry.
Was there an attachment of some sort? (there a big blank spot in your reply that is why I ask.)
Can you please attach your schematic and the error transfer function you are seeing?
We did not observe such a step…