Part Number: LM96080 We previously used the LM96080 to monitor the voltage of the CR2032 button battery, and we followed the datasheet recommendation to use the R1=22.1K and R2=30K divider resistor. However, it was later found that the current of this…
Part Number: LM96080 Hi, Good day. Our customer is using the LM96080 and they have a question regarding the calculation on negative voltage monitoring. ""I am using LM96080CIMT/NOPB in one of my project. I need to monitor a negative 2.5v voltage. I found…
Part Number: LM96080 Other Parts Discussed in Thread: LM96000 Hi
Customers want smaller packaging products, lm96080 packaging is too big
Is there a suitable product?
1. 1 set of smart fan 2. 3 sets of voltage detection 3. 1 temperature detection
hi
I read 0x7fc0 from the 0x21 register.Using the low 10 bits of this value to calculate, the monitored voltage is 4.8V, but in fact I expect the voltage to be 1.5V.I think I may have made a mistake somewhere, leading to such a big deviation between…
Part Number: AMC80 Hi team,
Customer wants to replace LM96080IMTX/NOPB with AMC80AIPWR, there are some several issues as below. Thanks a lot!
1. In the AMC80AIPW datasheet, there is 10mA input current as below. Is it the total current of device? If not…
Part Number: LM96080 Hi team,
When customer evaluates LM96080 device, they found the Logical "0" output voltage of open drain output only has the min value (0.4V) as below. Usually Logical "0" output should have max value. Could you please help to check…
Part Number: LM96080 Hi team,
My customer is using LM96080. They found a strange issue that, after powering-up and reading back 0x22h immediately, sometimes the return value will become 0 in the 1st time reading. Other times read value is always correct…
Part Number: LM96080 Hi Team,
My customer has 2 questions about LM96080:
1. what's the length of Value RAM of 20h to 29h? it is 1 byte or 2 byte(10 bit) value?
2. The read back ID register 0x3E value is 0x1A. But in Datasheet it should be default 0x01…