Part Number: LMC662 Other Parts Discussed in Thread: LPC662 , LMC6082 Hello,
I am looking to replace LPC662 SOIC8. It looks like the 2 closest drop-in replacement parts are LMC662, and LMC6082.
Does TI have a longevity supply program?
Can TI provide…
Part Number: LMC662 Hi, TI expert
There is a problem that the amplification rate is too different while the customer is using the LMC662AIM (OPAMP).
The test was conducted with 10 samples received a few years ago. Since the samples are old parts, I think…
Part Number: LMC662 I have an opamp circuit as shown below.
My board stack up is SIGNAL-GND-POWER-SIGNAL .
I am providing a polygon to Guard the trace which is going to non-inverting the input of the opamp.
The guard trace is connected to SMA connector…
Part Number: LMC662 Other Parts Discussed in Thread: LMP7721 Dear Team,
We need to measure the voltage from a charge pump that is present inside the ASIC.
The Impedance of the charge pump is 200T Ohm. The team has designed a circuit with LMC662A which…
Part Number: LMC662 Other Parts Discussed in Thread: TLV9002 Hello. I made a circuit with a voltage follower circuit with a single 5V power supply using LMC662.
When the input voltage exceeds about 3.5V, the output voltage jumps to 5V.
Is this suspected…
Hi Hari,
The valid input and output range of the LMC662 (or any amplifier) is determined by the exact value of the power supply voltages. See the absolute maximum rating is given relative to the supply voltages V+ and V-.
The valid common-mode input range…
Part Number: LMC662 Tool/software: WEBENCH® Design Tools Hi, I have drawn up a circuit to include LMC662A which was the closest I could find to LMC662 in TINA-9. But there are no specifications included with it, so for instance, I could according to the…
Part Number: LMC662 Other Parts Discussed in Thread: OPA134 Customer built hardware boards based on unity gain schematic below. Oscillation was observed. To make circuit stable, a 6.8KOhm pull up resistor was added at output of Op-amp.
However, customer…
Part Number: LMC662 I have a circuit that uses the LMC662 and in development, which used LDC HKAN parts, everything works as expected. However, when we went to production which used LDC 8CX7 parts, the performance of the circuit is very different. I've…