Part Number: LMG1210 Other Parts Discussed in Thread: TINA-TI Dear TI-development team, i am currently writing my bachelor thesis and would like to use the LMG1210 to control a switching amplifier in the half-bridge topology. Since only AWR models are available…
Part Number: LMG1210 Good day, colleagues,
My customer wants to use the LMG1210 with eGAN MOSFETs for power stage in a buck DCDC topology.
They need to do is sensing the inductor current for a current mode DCDC converter. Do you have some application or…
Part Number: LMG1210 Other Parts Discussed in Thread: LMG3100R017 Hi
I would like to design with the following specifications.
1. Gate Driver: LMG1210
2. GaN MOSFET: EPC2071 https://epc-co.com/epc/products/gan-fets-and-ics/epc2071
3.Motor Spec
- Motor…
Part Number: LMG1210 Hi,
I'm implementing SPWM with the help of LMG1210 gate driver IC. For my unique application, I've to go with switching frequency if up to 1.5MHz. That's why I've selected this IC.
Due to very low rise and fall time…
Part Number: LMG1210 The eval board of LMG1210 has EPC2001C and can switch up to 15MHz. Our design use EPC2055 and EPC2023 as upper and lower fets. EPC2023 has significantly higher gate charge. we want to switch at 10MHz. Do you think LMG able to drive…
Hey,
With GaN products, the layout and PCB design is critical, so this could very well help you in solving this issue. If after this PCB revision, the issue persists, please reply to this thread with updates and I can help further assist in a debug. Until…
Part Number: LMG1210 Hello,
I saw another post that I think answered this, but I wanted to ask explicitly. Is the LMG1210 suitable for driving the EPC2304 GaN FET? I'm in the process of designing a full-bridge Class D driver. So I'm thinking two LMG1210…
Hi Ritesh,
Thank you for your reply.
The customer was confirmed by LMG1210EVM.
At that time ringing was not large because the distance from the GaN FET was 5mm.
It could not output large power, the customer designed the PCB in LMG1210.
The distance to…