Hi Mostafa,
I have downloaded and tested the device model, I have not been able to replicate the error. Please delete the current file you have for the device model & test simulation. Then download the new one from the following link. https://www.ti…
Part Number: LMG3410R050 Hi Team, seeking for some inputs.
Topology is going to be a common-source bidirectional switch. Then, I don't have a low-side or high-side switch. The datasheet specifies those requirements for a half-bridge. Since I am going…
Part Number: LMG3410R050 Other Parts Discussed in Thread: LMG3410R150 Hello,
RD used GanFET with driver for Laser Diode switching.
The Rise time / Fall time of LMG3410R05 I found on TI website is the fast, but it still can not meet customer spec.
RD currently…
Part Number: LMG3410R050 Hi,
When I use TI LMG3410R050 GaN have some problems, hope you can reply.
I want to confirm the IC, so I use the double pulse test to measure it. To avoid damage to upper device in the third quadrant, so I use the SiC diode.
Then…
Part Number: LMG3410R050 Hello Can i Please get the Ids on vs Temperature curve for LMG3410R050. Datasheet seems missed that vital information. Aslo can you tell me how the normalized Rds on is calculated. Aslo i note that Ids rating stated as 12A at…
Part Number: LMG3410R050 Hello,
I have some questions about the fault detection of LMG3410R050. Besides OCP, OTP and VDD UVLO, I am wondering if the UVLO of LDO 5V and Vneg will trigger fault from the GaN device. Also, I would like to know the UVLO value…
Part Number: LMG3410R050 Other Parts Discussed in Thread: LMG3411R050 Hi there,
Except the handling of OCP events, is there any other difference between LMG3410R050 and LMG3411R050?
Thanks!
Part Number: LMG3410R050 Other Parts Discussed in Thread: LMG3410R150 Hi,
I am simulating the LMG3410R050 using PSpice for TI. There is Test_LMG3410_BUCK as a sample circuit in PSpice for TI. When I replace the LMG3410R150 in that circuit with the LMG3410R050…
Part Number: LMG3410R050 Hi,
I am trying to implement the LMG3410R050 in LTSpice using the PSipce library file supplied. I have generated a symbol however when I attempt to run the simulation it comes up with the following error:
The circuit i am trying…