Part Number: LMG5200 Other Parts Discussed in Thread: , LMG2100R044 TI support good morning
i plan to work with the LMG5200MOFT and have some questions.
1. VCC maximum current is 5mA, why evaluation board LMG5200EVM-02 has 1A LDO? can i use 50mA LDO?
…
Part Number: LMG5200
We made 500 pieces PCBA recently witch including 3 LMG5200 each. After SMT, we found almost 1/3 LMG5200 chips were shorted before power on, the short was betweent pin 1,8 and 9. The shorted chips looks normal without any a ppearance…
Part Number: LMG5200 Hello,
I'm an engineer designing a radiation-tolerant system for space. Our team likes the LMG5200 because GaN is more reliable than Silicon in space. The LMG5200 is also easy to work with because it has integrated driver stage a…
Part Number: LMG5200 Other Parts Discussed in Thread: LM5168
Hi team,
I am running a test for my inverter design using LMG5200 (similar to TIDA-00909 ) and I encounter short circuit between SW node and PGND instantly when I power up.
My design include…
Part Number: LMG5200 Hi, TI support team
The client company is reviewing the application of the LMG5200 to develop a beauty device.
- 7MHz HIFU (High-Intensity Focused Ultrasound) Transducer
- Operating Power of HIFU:16~20V, 2A
The circuit is composed…
Part Number: LMG5200 Hi Experts,
Seeking your assistance on this query:
This component is being used in a design to drive a 2-phase linear motor which can consume up to 9.4A (peak) per motor phase. It is configured for a switching frequency of 10kHz,…
Part Number: LMG5200 Hi team,
Could you help check if we get any GaN part support automotive class-D amplifier application?
Thanks and Best Regards,
Will
Part Number: LMG5200 Hi Team,
We would like to ask your help regarding our customer's inquiry below.
The requirement of our below circuit is to operate in pulsed mode and in CW ( continuous on) mode.
I completely understand the requirement for a …
Part Number: LMG5200 Other Parts Discussed in Thread: SN6501 , Hi Team,
This inquiry of our customer is related to the other thread below.
e2e.ti.com/.../lmg5200-bootstrap-capacitor
According to our customer,
We are using the circuit in pulse mode to turn…
Part Number: LMG5200 The part is marketed as a "10 A" Half-bridge power module. Yet, the abs. max. rating mention 10 A as the unconditional switch node current, which would turn it rather into a "5-6 A" half-bridge module when accounting for realistic…