Part Number: LMH0318 Other Parts Discussed in Thread: LMH0340 , LMH0341 Can i give common clock,data I2C interface for the following devices
lmh0341,lmh0340,lmh0318.
Part Number: LMH0318 Hello,
Is there any way I can get a sample of EOM data to verify the information I am receiving?
Additionally, the data I have received does not seem to be plotting an eye diagram; instead, it only displays four parallel lines.
Can…
Part Number: LMH0318
Hi Team,
i'm using LMH0318RTWR and controller is ESP32. i'm facing difficulty in writing data and reading data from it's registers
#define LMH_ENABLE 25
#define LMH_MOD_SEL 26
#define LMH_CS 5
#define MISO_PIN 19
#…
Part Number: LMH0318 Other Parts Discussed in Thread: LMH0324 , DS25CP104A , Hello,
we have developed a 3G-SDI switch with the following TI components:
Equalizer: LMH0324
Switch: DS25CP104A
Reclocker/Cable Drive: LMH0318
If I power on the device without any…
Part Number: LMH0318 Other Parts Discussed in Thread: LMH0397 , LMH0324 Hello,
Is there an existing linux kernel driver for LMH0318 device ?
Regards,
Bruno
Part Number: LMH0318 Hallo,
I'm confused about reading registers using the I2c/SMBus.
Reading the SNLU183 I see that write into a register should use the followin protocol:
|RAW | Register Address | Register Content | Register Mask |
So using the…
Part Number: LMH0318 Other Parts Discussed in Thread: LMH0324 , SIGCONARCHITECT , USB2ANY , LMH1218 Hallo,
I'm using the LMH0324-18EVM to test the LMH0324 and LMH0318. Now I need to use the LMH0318 with non default configuration.
Is there any tool available…
Part Number: LMH0340 Other Parts Discussed in Thread: LMH0318 I am looking for advice for connecting an LMH0340 to an LMH0318 via 12" of 100Ohm twisted pair. The output of the 0340 is set to 100Ohm diff, but is there anything special I should do…
Part Number: LMH0318 I wish to use this part solely as a driver, not a mux, so I only need one of the inputs and one of the outputs. My question is what, if anything, I need to do with the unused ones. Currently I just have them floating, but I can pull…
Part Number: LMH0318 Other Parts Discussed in Thread: LMH1219 , LMH1218 , LMH1297 Hallo,
I'm confused about reading registers using the I2c/SMBus.
Reading the SNLU183 I see that write into a register should use the followin protocol:
|RAW | Register…