Part Number: LMH0318 Other Parts Discussed in Thread: LMH0324 , SIGCONARCHITECT , USB2ANY , LMH1218 Hallo,
I'm using the LMH0324-18EVM to test the LMH0324 and LMH0318. Now I need to use the LMH0318 with non default configuration.
Is there any tool available…
Other Parts Discussed in Thread: LMH0324 , LMH0318 Dear Technical Support Team,
I have a question about LMH0324-18EVM.
I can't find datasheet of LMH0324-18EVM. I'd like to see schematic of this board.
How can we get it? Is it based on NDA?
http…
Hi Satoshi-san,
I was actually thinking the same thing as you.
When the LMH1297 is used in EQ Mode and SDI_OUT is enabled, there may be cross-talk from SDI_OUT that interferes with the input on SDI_IO at maximum cable reach. To test whether this is the…
Hi Bogey,
Yes, that is one possibility.
Another possibility is to use the LMH0324 (Cable EQ) + LMH318 (Cable Driver + Reclocker), which uses more updated device architecture for implementing SDI distribution network, and the LMH0324-18EVM is available…
Hi Mark,
Good observation. The LMH0318 and LMH1218 both have an integrated return-loss network, so it is not required to implement a return-loss network if you are hard-pressed for space on the board.
However, with that having been said, we have observed…