Hi Aviad,
Thanks for your question. It is a good idea to match the P and N of SDI_OUT if possible, but not doing so will not have a significant effect on return loss and other signal integrity specifications.
Our own EVM design does not match the LMH1297…
Part Number: LMH1208
Thank you for listening. I have obtained the LMH1208 programming guide, but I still need some program assistance. Can you provide a reference code to configure the chip, such as using In to receive data and then SDI_ I only…
Part Number: LMH1219 Other Parts Discussed in Thread: LMH1208 , Hello,
I have an application that need to use EQ for HD-SDI from 1 signal to 4 signals and I need an advice which option is better.
for what I can see there is 2 options which the LMH1219 …
Part Number: LMH1297 Other Parts Discussed in Thread: LMH1219 , LMH1208 , , LMH1228 , LMH1218 Hello,
Our customer is looking for LMH1208 and LMH1219 single chip solution product. Then he has a question if LMH1297 can work as 12G UHD-SDI driver and 12G UHD…
Part Number: LMH1228 Other Parts Discussed in Thread: LMH1208 Hello,
Our customer complained he could not down load the programming guide (SNAU206) from the web site, even though he had accessed the down load site.
Could you kindly help him to down load…
Part Number: LMH1208 I have seen many applications of the SDI interface and I understand the termination schemes of transmitting over a single coax and terminating the other output capacitively into 75 ohm. The same is then done at the receiver.
However…
Part Number: LMH1208 Dear support team,
Would you share your mailing list for sending email, because I'd like to ask questions with my confidential information?
Best Regards,
Katsumi Maeda
Part Number: LMH1208
Hello,
Customer wants to use RS-170(NTSC/PAL) input and make 4 outputs as below diagram.
Is it possible to make this configuration?
If above configuration is available,
1. Can select LMH1208 output as 12G, 3G, HD or SD?
2. Can use…