Part Number: LMH6401 Other Parts Discussed in Thread: TINA-TI Hi Team, I found the simulation from Roey: LMH6401: Simulation Error on LTSPICE
https://e2e.ti.com/support/amplifiers-group/amplifiers/f/amplifiers-forum/1167241/lmh6401-simulation-error-on-…
Part Number: LMH6401 Hi Team,
I would like to address the LMH6401 SPI via opto coupler
The operating frequency is 10KHz
I saw that the LMH6401 specifies only maximum frequency. Is there any minimum frequency limitation?
Best regards.
Part Number: LMH6401 I am referring to the old post --> LMH6401: Need DC offset drift information
Can I request for the DC offset drift information and data as well?
I will be using the LMH6401 for DC-coupled application.
Thank you,
Regards,
Sek…
Part Number: LMH6401 The following files contain S-Parameters for the LMH6401 at three gain settings (Max gain, 10dB, and -6 dB).
LMH6401_MaxGain_Vs=5V.s4p LMH6401_Gain_10dB_Vs=5V.s4p LMH6401_Gain_-6dB_Vs=5V.s4p
Part Number: LMH6401 Hi Team
i am using the PSPICE model of LMH6401 and simulating it in LTSPICE
What are the B0 - B5 ports? How do i connect them?
How can i choose the gain?
Please help in advance
Regards,
Roey
Part Number: LMH6401 Hi,
Is it possible do daisy chain 32~64 of these in the same SPI bus. The Sclk and SDI is tied. What is the current for these pins?
Thanks,
Vicky
Part Number: LMH6401 Other Parts Discussed in Thread: SN74CBTLV3251 Hi,
I would like to daisy chain 64 of thes parts on the same SPI bus direct tie the SCLK and SDI pin together with separate independent CS and SDO. Is it possible? Can you tell me the…
Part Number: PSPICE-FOR-TI Other Parts Discussed in Thread: LMH6401
Hello E2E Experts,
I'm not sure if this is the best place to report this bug but the PSpice TI Component Library database has an issue with the LMH6401 Model Test Circuit. It refers to…
Part Number: LMH6401 Hello Team,
can you confirm that the voltage levels for the SPI interface always are 1.8V (high) and 0V (low) no matter if unipolar or bipolar power supply is used, please?
VS- = 0V connected to GND
VS+ = 5V
SPI-Bus voltages are referenced…