Part Number: LMH7220 Hi,
I want to utilise LMH7220 component in my design. For design validation I require the Spice model of the same.
Thanks in Advance.
Part Number: LMH7220 Other Parts Discussed in Thread: TLV3604 Hi,
I would like to utilise LMH7220 in my design based on specifications mentioned in its datasheet. For design validation, I require the spice model of the same. Request you to please share…
Part Number: LMH7220 Looking for some help clarifying the input current draw (e.g. impact on a reference voltage supply) for something like a mid-point supply on Vin- and a full-range swing at Vcc=12V (Vin+_min = 0V; Vin+_max = Vcc-2 = 10V; Vin- = fixed…
Part Number: LMH7220 Hello,
I would like to ask what is the input impedance of LMH7220 on both positive and negative input?
I am trying to use it in a 50ohm matched system.
Best regards,
Albert
Part Number: LMH7220 Other Parts Discussed in Thread: BUF602 Hi,
I am trying to figure out a buffer or comparator for my high speed sensing circuit.
The short propagation delay of LMH7220 seems pretty good for me. However, I'd like it has very low input…
Part Number: LMH7220 Hi,
I have questions regarding the LMH7220.
- Can the GND pin be connected to a -12V supply?
- What will the output be referenced to?
- Can the negative input be driven with a bipolar input?
Thanks! Lauren
Part Number: LMH7220 Other Parts Discussed in Thread: TLV3501 Hello,
I would like to use the LMH7220 to design a high-precision PWM system. The inputs are a sawtooth signal and the signal to be encoded. I will use a configuration with hysteresis.
However…
Part Number: DS90LV047A Other Parts Discussed in Thread: SN65LVDS20 , SN65LVDS31 , SN65LVDS105 , LMH7220 , DS90LV001
Hello,
For a high precision (<10ps) TDC application I am looking for a way to translate LVTTL and TTL signals to LVDS signals without adding…
Part Number: LMH7220 Hello,
The hysteresis example on page 20 of the LMH7220 data sheet depicts a typical single ended comparator topology.
For the same input topology but for LVDS differential outputs how would the hysteresis feedback be connected?
…