Part Number: LMK03318 Dear Team,
The maximum value of LVCMOS input high voltage is VDD_IN.
If an overshoot occurs and exceeds VDD_IN, will this IC stop functioning?
Many Thanks,
Ryo
Part Number: LMK03318 Dear Team,
The swing specification for LVPECL that you recommend is 500~1000mV. We have an IC whose specification is 0.4~0.9V Is this output swing adjustable?
Many Thanks,
Jimmy
Part Number: LMK03318 Hi, I could not find any information on dimensions of the part LMK03318RHST (Package WQFN (RHS) ) in the datasheet or website. Please help to get the information.
Part Number: LMK03318 HI Support,
I am using TICSpro to generate configuration file for the LMK03318.
I am trying to come up with PLL filter parameters and failing - please help.
Datasheet (SNAS669E –SEPTEMBER 2015–REVISED APRIL 2018) indicates to use …
Part Number: LMK03318 Other Parts Discussed in Thread: CDCI6214 , CDCI6214EVM
Hi,
I am using the LMK03318 to generate several differential outputs. But the output7 peak to peak swing is always larger than other output. The swing is almost about 2V that…
Part Number: LMK03318 Hi,
I am using LMK03318 to generate several AC-coupling LVDS clocks to one controller. Right now, two reserved clocks are not useful. Should I disable the two outputs or continuedly to generate clocks from that two output? Which…
Part Number: LMK03318
Hi,
I am using the LMK03318 IBIS for a clock simulation. I am using a simple AC-Coupling way to connect the LMK03318 output to my controller. It has a 1.2V bias Vcm on the controller side.
In the LMK03318 data sheet. The differential…
Part Number: LMK03318 Hey,
We would some help to understand how we can change the base adresse.
We have everything configured and its working as expected - we create a epr which we are using to program the pll.
According to the datasheet we would need…
Part Number: LMK03318 HI Support,
1) Is "Export HEX register values" file generated by TICSpro the correct production programming file that should be used to program LMK03318 in production on virgin boards (using onboard I2C bus master for example…
Part Number: LMK03318 HI
Are device function parameters and reliability NOT AFFECTED if device would operate driven by LVCMOS 3.3V 25MHz oscillator 50R output impedance connected to the PRIM_P input of LMK03318 configured as shown below:
Thank you, …