Hi Sameeksh, No problem I understand.
Once you have powered up, to pick page 1 of EEPROM, follow the steps listed below under the programming section of the LMK03318 DS:
R145[3:0] should be set to 1'b to select page1.
GPIO pins are checked on power…
Part Number: LMK03318 Other Parts Discussed in Thread: USB2ANY Hello, support team.
I have a question. Whad do you mean min of I2C Clock Rate is 100kHz and max. is 400kHz?
Refer see below LMK03318 datasheet, please. https://www.ti.com/document-viewer/LMK03318…
Part Number: LMK03318 HI,
Can i know if there is a configurable settings for LMK03318 that set the Out0-Out5, to output a fixed 100Mhz LVDS output ?
tx
rdgs
stloh
Shu,
I have the following responses:
the primary input is an LVPECL clock, the secondary input is a LVCMOS clock from an active oscillator. Both frequency is 100MHz. Do I need to transfer the LVCMOS clock to LVPECL to secondary input? But use the auto…
Part Number: LMK03318
Hi,
Below is my applicaiton schematic for LMK03318, the device is programmed for the LVPECL output of 500MHz
I am using register programming straight away to see the clock output
I have a found a minor glitch, i am not sure why…
Part Number: LMK03318 I have a question. What is the maximum input voltage spec for the PDN of LMK03318?
Datasheet chap. 8.20 "2-Level Logic Input Characteristics" says only the minimum spec.
https://www.ti.com/document-viewer/LMK03318/datasheet…
Part Number: LMK03318 Hi,
I want to perform simulation using LMK03318 as driver & for that purpose i need IBIS model of this clock generator. Please provide the model.
thanks
Part Number: LMK03318 Hello,
1. Will the PLL unlock when the reference input is auto switched from secondary to primary in datasheet Figure.43?
The flowchart in Figure.44 describe that the PLL shall unlock momentarily when the mux auto switch to secondary…
Just a follow-up here for anyone reading this later. The root cause is that because the LMK chip is behind a mux, the default state for the Linux kernel i2c driver is to close and open the mux between any transfer. This opening and closing is acceptable…
Hello Kadeem-san,
Sorry for long time no reply. I see, that's why you recommend setting it to 1. I understood very well.
By default settings, always-on clock is set to OFF, LMK03318 can receive a differential signal. If the input signal is a single…