Part Number: LMK04832EVM Other Parts Discussed in Thread: LMK04828 , LMK04832 Hello,
I looked on EVB schematics both LMK04828 and LMK04832 and put attention that external VCXOs' outputs are connected to LMKs' OSCin inputs with opposite polarity, i.e. negative…
Part Number: LMK04832EVM Other Parts Discussed in Thread: LMK04832 Hi team,
I want have two clocks with LMK04832EVM , one is 6.25M ,another is 16×6.25M 。and the two clocks have 90° phase difference.can you show me how to configure it. thanks.…
Part Number: LMK04832EVM Other Parts Discussed in Thread: LMK04832 Hi ,
To understand how the LMK04832 works, we have the evaluation card that Ti offers. (VCXO 122.88 MHz)
I would like to use the LMK04832 in "holdover" mode and I would like a little more…
Part Number: LMK04832EVM Other Parts Discussed in Thread: LMX2820 , LMK04832 , CDCE6214 Hello,
I need something to take a 10MHz clock input and generate 5 x 100MHz clocks that are all in phase.
I This evm capable of doing this or do I need something like…
Part Number: LMK04832EVM Other Parts Discussed in Thread: LMK04832 Hi Ti Team,
Can you please let us know the requirements to get good phase noise and good slew rate 3GHz CLKOUT signal(CLKin1=100MHz, VCO=3GHz, Divider=1, Duty cycle correction bit enable…
Part Number: LMK04832EVM Other Parts Discussed in Thread: ADC09QJ1300EVM , Hello team,
For a demonstration of the ADC09QJ1300EVM, I need a reference clock of 1.3GHz.
Unfortunately, I do not have a dedicated clock generator.
I would like to use the LMK04832EVM…
Part Number: LMK04832EVM Other Parts Discussed in Thread: USB2ANY , LMK04832 To program the LMK04832EVM, TI recomends using the TICS Pro software and the USB2ANY. However, I would like to program it using a smaller device, like a raspberry pi. Does anyone…
Part Number: LMK04832EVM Other Parts Discussed in Thread: LMK04832
Hi TI Team,
Is it possible to get Phase synchronization among CLKout signals in below scenario?
CLKin1 reference signal is 100MHz , VCO2 is 3000MHz and using clock divider 15 the all CLKOUT…
Part Number: LMK04832EVM Other Parts Discussed in Thread: USB2ANY , LMK04832 TICS Pro uses the USB2ANY device (HPA665) to write to the registers of LMK04823EVM. I would like to create a Python script that does the same. I have the TICS Pro saved file and…