Part Number: LMK61E07 Other Parts Discussed in Thread: LMK61E2 , Hi team,
What is the function of these register bits (SWR2PLL, AUTOSTART and ENCAL)? How to use them?
Does both the AUTOSTART bit and the ENCAL bit have a function to trigger PLL Lock?
F…
Part Number: LMK61E07 Other Parts Discussed in Thread: LMK61E0M , LMK61E2 Hello,
I am trying to validate if LMK61E07 can be used to generate 1 GHz CLK or not.
As far as I understood from the TICS Pro SW, it looks like 1 GHz CLK output is not possible …
Part Number: LMK61E07 Other Parts Discussed in Thread: LMK6H Hi team,
I'm looking for the right clock generator or oscillator for the customer with HCSL low-jitter 400MHz output. Their looking for an oscillator for their SoC. I think LMK61E07 may fit…
Part Number: LMK61E07 Other Parts Discussed in Thread: LMK61E2 , LMK62A2-100M HI.
I want to control LMK61E07 using AVR.
I want to output 100MHz LVDS.
Can I get an I2C C code example?
Thanks.
Part Number: LMK61E08 Other Parts Discussed in Thread: LMK61E07
Hi support team,
Please let me know the difference between LMK61E08 and LMK61E07.
Regards, Dice-K
Part Number: LMK61E07 Other Parts Discussed in Thread: LMK61E08 Hi Expert,
Customer used our LMK61E07 for BCM65408 70.656Mhz clock and its spec mentioned like below < 1Hz
However, from their measurement, the stability 3.66Hz looks failed. Would you…
Hi Jatin,
The TIDA-00626 reference design uses LMK61E2 which has a different footprint compared to LMK61E07 and LMK61E08, so if you are using the gerber and PCB files from the reference design you will need to use LMK61E2.
LMK61E2:
LMK61E07/E08:
If…
Hi Pawel,
What output frequency and tuning range do you need? From what I understand, you need glitchless output while output frequency changes, is that right? As for devices that support frequency margining, CDCE6214-Q1, LMK03318 and LMK05318 are featured…
Part Number: LMK61E07 Hi,
we are designing an audio product where LMK61E07 will be a master clock synchronized to an external clock, much like as it is described in the DCXO section. We shall do fine tuning on a continuous basis and some bigger changes…
Part Number: LMK61E07 Other Parts Discussed in Thread: USB2ANY , LMK61E2 How do you program the LMK61E07? The evaluation board does not have a USB2ANY interface, and the LMKxx software tool
does not include the LMK61E07 as a device option. The development…