Part Number: LMP90100 Other Parts Discussed in Thread: LMP90080 , ADS124S08 Hi Team,
My customer was using LMP90100 before. Due to the short supply of LMP90100, my customer's production line has been suspended.
It is emergency that recommend an new device…
Part Number: LMP90100 Other Parts Discussed in Thread: ADS124S08 Hi,
Are the GPIO pins D0-D6 CMOS inputs?
We would like to know if there could be issues with leaving them floating, when configured as inputs, such as indeterminate states and ESD damage…
Hi Noah Pierce,
The LMP90100 does not have internal pull-up / pull-down resistors on the GPIO pins. You should also not let these pins float. Tie each pin to some voltage level (either GND or VIO). You can also set the GPIOs as digital outputs, where…
Part Number: LMP90100 Other Parts Discussed in Thread: ADS124S08 Is there a sample code to program the LMP90100 with any processor other than the MSP430?
At the same time, can you share with me if there are sample codes for measuring and calculating the…
Part Number: LMP90100 Other Parts Discussed in Thread: ADS124S08 I want to read values from 2 RTDs using LMP90100 AFE software. But it cannot separate the current sources as two different channels. If I make another connection like 3-Wire RTD using…
Part Number: LMP90100 I try to program the LMP90100 with the help of the PIC24F series. I use SPI as a type of communication. However, I have a problem with the fact that the examples for LMP90100 are already written on MSP430. Where can I find the LMP90100…
Part Number: LMP90100 I was wondering what the acquisition time or integration time of the AFE is based on the ODR. Do lower ODRs provide more acquisition/integration(/averaging) proportional to the rate? Something else? Is there any variation or description…
Part Number: LMP90100 Hello,
we are using LMP90100 since 2011 (former National Semiconductor) with introduction in one of our devices in 2012 but now we are facing a problem we have never seen before:
we are working with ScanMode0: single-channel continuous…
Part Number: LMP90100 Dear Sir or Madam,
In one of our devices we use 96 LMP90100.
The LMP90100 is configured for multiple channel continuous conversion. We are facing problems using the LMP90100 near the external climate chamber temperature of -40…