Part Number: LMR14030-Q1 Other Parts Discussed in Thread: LMR14030 , LM5149 I would like to use LMR14030SQDPRTQ1 for making +12V, 2A power supply.
I have one requirement in the circuit that if 12V input is given to IC, the output should be 12V. Is this…
Part Number: LMR14030-Q1 Hi team,
Is there any concern if I use 0.22uF as Cboot of LMR14030-Q1 while 0.1uF is recommended?
Could you please advise the maximum value I could use for Cboot?
regards,
Part Number: LMR14030-Q1 Other Parts Discussed in Thread: LM63635-Q1 , LMR14030 Hi, Can you confirm whether LMR14030-Q1 is equivalent to ASL B rated IC. If not, could you please explain why not? Could you recommend and ASIL rated IC with the same/EMI per…
Part Number: LMR14030-Q1 Am I correct in thinking that when Webench reports a negative gain margin, it actually means the gain is negative at the phase crossover and therefore (GM (dB) = 0 - G(dB) @ phase crossover) the system has a positive gain margin…
Part Number: LMR14030-Q1 Hi Team,
We know from DS that IQ=40uA(typ) when Tj=25C.
Customer consulted us when Tj=85C, roughly, what value will IQ become?
Kindly help to advise. Thanks.
Best regards,
Terry
Part Number: LMR14030-Q1 Other Parts Discussed in Thread: LMR14050 Hi, TI Support Team
I am trying to configure USB CAHRGER as below BLOCK.
Previously, two LMR14030-Q1 products were used as INPUT of USB CHARGER IC, but to reduce to one, the block is…
Part Number: LMR14030-Q1 Other Parts Discussed in Thread: LMR14030 Please help to provide calculation or Formula for minimum startup voltage.
for example, the output voltage is set to 3.3V or 5V, what is the input voltage will be able to gerenate 3.3V…
Part Number: LMR14030-Q1
Hi Team, seeking your assistance.
Encountering a large spike immediately upon plugging in Vin, long before the LMR14030-Q1 has started switching.
Webench project
https://webench.ti.com/appinfo/webench/scripts/SDP.cgi?ID=5D03…
Part Number: LMR14030-Q1 Other Parts Discussed in Thread: TPS54388C-Q1 , LMR14030
Hi Expert,
Our customer use LMR34010 and TPS54388C-Q1 in the same design. Since there is no MCU in system, they would like to connect PG form LMR14030 to EN pin of…