Part Number: LMR14050SEVM Hi team,
I use LMR14050sEVM and change vout for 10.8V, Vin=12V; and use feedforward capacitor 680pF to optimization loop, reduce the fluctuation of output voltage during load dynamic.
But there is a platform for the measured…
Part Number: LMR14050SEVM Hi,
I am using LMR14050SEVM and noticed that evaluation board is specked at 7V input minimum but IC is capable of up to 4V input. When I apply 7V input with a 4A load at 5V, output starts cycling from 0V to 5V. and Inductor…
Part Number: LMR14050SEVM Other Parts Discussed in Thread: LMR14050 Hello.
LMR14050SEVM is implemented on 4-layers PCB.
Is it possible to use a 2-layer PCB-layout for LMR14050?
Hi Cho,
Yes, this device can step down 12V to 5V @ 5A. Please see section 9 in the data sheet along with WEBENCH for a reference design to achieve your requirements. You can also use the dedicated EVM. Please enter your specific application requirements…
Part Number: LMR14050SEVM Tool/software: WEBENCH® Design Tools Hello,
I am currently doing work with the LMR14050SEVM, and it would be very helpful if there was a CAD file/model available for evaluation. Would it be possible to receive a CAD model or…
Part Number: LMR14050 Hi Experts,
Good day! Our customer need your expertise on their design. Kindly please help to verify. Here is the full details below.
we are planning on using the LMR14050QDPRRQ1 to carry out the following: Convert 12-24VDC to 5VDC…
Part Number: LMR14050SEVM Are the gerber files for the LMR14050EVM available? Can I send them directly to my customer?
Thanks for your help with this!
Richard Elmquist
Part Number: LMR14050SEVM Tool/software: WEBENCH® Design Tools I'd like to know if a Webench or Tina circuit (simulator netlist/input deck) based on the LMR14050SEVM Evaluation Module (EVM) has been built by TI and can be loaded by a user as a starting…