Part Number: LMR16006 Hi Katelyn,
Another LMR16006 question.
With respect to over current or short circuit at the output, am I correct in my understanding the at the device will likely enter shutdown due to temperature increase at that point?
And that…
Part Number: LMR16006 Hello,
I am using LMR16006YDDCR based upon a WEBENCH design (thanks for that!). I have a question that will help in finalizing my design.
1. According to the datasheet, if SHDN is not to be utilized, installing a 100K resistor…
Part Number: LMR16006 Hi, please could you tell me if it's safe to apply external voltage to the output of the buck converter with no input voltage?
I have added a diode in series with the input to prevent the reverse current flow, as recommended in…
Part Number: LMR16006 Hello!
Our DRV832xR uses an internal LMR16006X to provide a buck output in case the customer wants it.
Some customers buy the Buck included version but won't be using it at all.
I have been told by some that simply routing…
Part Number: LMR16006Y-Q1 Other Parts Discussed in Thread: TPS54360-Q1 Hi Team,
LMR16006-Q1 and TPS54360-Q1 was used for customer project. It's a urgent case.
At first, they have some EMI issue, See detail information in attachment.
Customer decide…
Part Number: LMR16006 We have several designs using LMR16006 as a switching pre-regulator from 7-40V input (nominal 12V) down to 5V.
During EMC qualification testing we have seen some issues with RF Immunity susceptibility in the product between 200…
Part Number: LMR16006 I'm having an FCC radiated and conducted noise issue. Can anyone give me tips on passing FCC? Also, I'm really interested if anyone has passed FCC with the LMR16006X (700Mhz) device.
Part Number: LMR16006
One of Schneider's products uses "LMR16006". The ECO mode creates audible noise with ceramics that customers complain about. Does TI offer a pin for pin replacement for "LMR16006" that is not afflicted with "ECO mode"?
Hello Katelyn,
thanks for your appnote, this at least confirms my initial thoughts on what was going on.
The only thing that remains now is that I dimensioned my circuitry based on the output of webBench for this design. The datasheet of the LMR16006…
Part Number: LMR16006 Other Parts Discussed in Thread: TPS54360B , Hello
I am using two LMR16006Xs to generate 5V 250mA and 12V 100mA. The input voltage is 36V. I am also using TPS54360B to generate 24V 0.8A. The figure below shows the shunt down waveform…