Part Number: LMR34206-Q1 Hello,
In the datasheet of LMR34206-Q1, the bootstrap capacitor is listed as "high-quality ceramic capacitor of 100 nF and at least 16 V". We considered a 100nF/16V/0402/X7R/10% tolerance capacitor in our design.
In…
Part Number: LMR34206-Q1 Hi Experts,
LMR34602-Q1 is under evaluation on customer side. Could you provide Functional Safety FIT Rate, FMD and Pin FMA of LMR34206-Q1? So customer can evaluate the system failure rate. Thanks.
Best Regards
Songzhen Guo
+86…
Part Number: LMR34206-Q1 TI BU team,
we see two different recommendations for the PG pin in the documentation of LMR34206-Q1 :
Datasheet section 6 – „ if the function is not needed, Can be open or grounded when not used.“
Datasheet…
Part Number: LMR34206-Q1 Hello team,
1. What is the maximum power dissipation that the IC can withstand at 70-80 deg ambient?
2. Can this be used during cold cranking condition - 5.5 V i/p and 5 V o/p?
Thank you!
Part Number: LMR34206-Q1 Hi team, I have some questions regarding the operation of the LMR34206:
EMC Performance. There are 2 versions of LMR34206, one with FPWM and the other one has an auto mode for light loads. In general, which one of these 2 modes…
Part Number: LMR34206-Q1 I am performing a design with the LMR34206-Q1 with the following requirements:
Input voltage: 8,6V to 18V. Up to 42V in transient
Output voltage: 5V
Max. Output current: approx. 250mA
I hope you could clarify some design concepts…
Part Number: LMR34215-Q1 Other Parts Discussed in Thread: LMR33630-Q1 , LMR33620-Q1 Hi,
I have some questions regarding the devices LMR34215 and LMR34206 with 5V output and no FPWM:
Would they both work under the same output inductor and capacitance? I…
Part Number: LMR34206-Q1 Other Parts Discussed in Thread: LMR34215FSC5EVM Hello,
For LMR34206FSC5RNXRQ1 could you provide the efficiency about Vout=5V?
We only find the Vout=3.3V efficiency in datasheet.
Regards,
Dongbao