Part Number: LMR36006-Q1 Hello,
I would like to ask you a question about LMR36006-Q1. RNX0012B and RNX0012C have information on EXAMPLE BOARD LAYOUT and EXAMPLE STENCIL DESIGN in the data sheets, but there are some differences. It also states that the thickness…
Part Number: LMR36006-Q1 Hello,
I am considering the LMR36006-Q1 device. I would like to check the constants of peripheral components on WEBENCH, but according to my specifications, Vout=12V. WEBENCH is fixed at Vout=3.3V for some reason. Is there a way…
Part Number: LMR36006 Hello,
LMR36006 datasheet Section 8.2 shows the block diagram for this IC and AGND and PGND is shown to be connected internally.
If this is the case, what is the purpose of connecting the AGND and PGND externally ?
Also the layout…
Part Number: LMR36006 Hi,
I am having an issue with the part LMR36006FSC3RNXTQ1.
I am using it to lower the 24VDC voltage to 3.3V and 0.15A.
I am measuring a case temperature of 70C with ambient temperature of 25C.
I have looked into the Flip Chip temperature…
Hi Antoine,
You are welcome.
Here are a couple articles on CMC theory with a sub-topic on compensation ramp.
https://www.ti.com/lit/an/snva555/snva555.pdf?ts=1696861560942&ref_url=https%253A%252F%252Fwww.google.com%252F
https://www.ti.com/seclit/ml…
Part Number: LMR36006-Q1 Hi,
I am having an issue with the part LMR36006FSC3RNXTQ1.
I am using it to lower the 24VDC voltage to 3.3V and 0.15A.
I am measuring a case temperature of 70C with ambient temperature of 25C.
I have looked into the Flip Chip temperature…
Part Number: LMR36006-Q1 Hello Team, enclosed a simulation which do not fit do real measurement. Please could you help to optimize it. Many Thanks Josef
---
Our simulation schematics is as below.
Simulation results are as below.
1)Inductor Current
…
Part Number: LMR36006-Q1 Hi team,
I am using LMR36006-Q1 IC in my project. I chosen components based on the equations provided in the application chapter.
I have one question about the BOOT capacitor, VCC pin capacitors.
What is the impact on the output…