Part Number: LMR62421 I would like to simulate a 5V and 7V supply each using an LMR62421. The input voltage will range from 3.7V to 5.0V. Each supply is designed to drive 0.15A.
When I attach the LMR62421X_trans model to the part in the simulation, I…
Part Number: LMR62421
I used the LMR62421X_TRANS model in my design, it is giving me this error ERROR(ORNET-1019): Pin 1 in template not found on U1
(U1 is the part reference)
Part Number: LMR62421 Other Parts Discussed in Thread: LMR62014 , TLV61048 Hi,
I would like to ask some quetion about Vout setting. Setting parameter is the following,
Vin=3.3V Vout=15.11V R1=10kohm R2=110.4kohm
When I tried to operate LM62421 with that parameter…
Part Number: LMR62421 Other Parts Discussed in Thread: TLV61070A , TLV61048
Hi, this is volkan Greetings from Istanbul. In my application I need these two fixed DC differential voltage sources to pass the rail to rail level in an opamped circuit where I…
Part Number: LMR62421 Hi everyone, I have a circuit that uses a LMR62421 as power supply, I show you the design:
VBAT1 is the voltage of a battery and 7V should appear on the output, but VIN appears on VOUT, it is as if the circuit did not work, I replaced…
Hi Brian,
The "stage 2", or "phase 2", is not a classical concept defined in books. I just used it based on the motor behavior from rest to stable status of fast spin, and the current waveforms you provided.
I don't think the Cout…
Hi Zuhaib,
The max output will be larger than 5A. Here is the calculate method for your reference.
Will you consider TPS61033? It should be a better choice.
Regards
Lei
Part Number: LMR62421 Other Parts Discussed in Thread: LM2735 Hi,
I am seeing 3.3V on the output of the LMR62421 with the enable is low. The voltage seems to be a diode drop value of the input voltage so I am not sure what is going on. I have attached…
Part Number: LMR62421 Other Parts Discussed in Thread: LMR64010 , I am using LMR62421XMF/NO regulator to boost from Li ion battery 3.7 V to 12V . I had checked the switching output but no pulsing i can see .
Also i am cascading two boost regulator . In…