Part Number: LMS4684
Circuit working:
1.COM1 and COM2 are Shorted through the circuit
2. if IN1=0V, then the OUT1 is connected to 5V through the NC1, however, if IN1=+3.3V, then the OUT1 is connected to GND through the 100k Resistor.
3. The IN2 is controlled…
Part Number: LMS4684 I am looking for the maximum operating junction temperature for this component. It has an absolute maximum junction temperature of 150°C listed in the spec sheet, however I am looking for max operating.
Thanks
Part Number: TMUX1248 Other Parts Discussed in Thread: LMS4684 , TPS2116 , TPS22976 Hello,
The customer is looking for an analog switch that meets the following requirements.
Could you please recommend a suitable device?
- Switch type : SPDT, DPDT
- Supply…
Other Parts Discussed in Thread: LMS4684 , TS5A23159 Regarding the analog switch product LMS4684, a customer asked, what is the Frequency response of the switch? i did not see this documented in the datasheet.